Does the FRDM-KE06Z have a built-in CAN transceiver?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the FRDM-KE06Z have a built-in CAN transceiver?

839 Views
antonio_estupin
Contributor I

I read on the documentation provided online that it does have a CAN module, but could not find any information about whether it has a CAN transceiver or not?

Or do i need to buy one separately?

0 Kudos
Reply
3 Replies

755 Views
mjbcswitzerland
Specialist V

Hi Antonio

U7 on the board is the SN65HVD230D (Can transceiver), connecting the CAN_TX/CAN_RX lines to J11.

This chip is mounted on the board but J11 is not, therefore you just need to add the three pin (0.1") header to use it.

Regards

Mark

Complete Kinetis solutions, training and support: http://www.utasker.com/kinetis.html
Kinetis KE:
- http://www.utasker.com/kinetis/FRDM-KE02Z.html
- http://www.utasker.com/kinetis/FRDM-KE02Z40M.html
- http://www.utasker.com/kinetis/FRDM-KE04Z.html
- http://www.utasker.com/kinetis/FRDM-KE06Z.html
- http://www.utasker.com/kinetis/FRDM-KE15Z.html

0 Kudos
Reply

755 Views
antonio_estupin
Contributor I

Thank you for the quick response,

So just to be sure, there´s a CAN transceiver and a CAN controller integrated in the microcontroller right?

Sent from Mail<https://go.microsoft.com/fwlink/?LinkId=550986> for Windows 10

0 Kudos
Reply

755 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Antonio:

The KE06Z MCU only has CAN controller, no transceiver.

But Frdm-ke06z has a transceiver, U7, as mark mentioned.

Regards

Daniel

0 Kudos
Reply