Hi everyone,
I have a Kinetis KL25Z evaluation board with MKL25Z128VLK4. Does this MCU support flash swap feature?
Thanks
Tuo
解決済! 解決策の投稿を見る。
Hello Tuo Wang:
KL25 MCU only contains 1 flash block, and it does not support flash swap functionality. For firmware update purposes (e.g. bootloader), the flash programming routines need to be run from RAM memory.
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Tuo Wang:
KL25 MCU only contains 1 flash block, and it does not support flash swap functionality. For firmware update purposes (e.g. bootloader), the flash programming routines need to be run from RAM memory.
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Jorge,
We are currently using an MK60DN512, but due to its difficulty to source, we are considering using the MK60DN256ZVLL10 and urgently need to know if the flash swap feature is supported in the DN256 as this is critical to our application.
Also, do you know what the "Z" refers to and what Errata may exist for that part (DC 2019+).
Thank you!
Thank you, Jorge! That's very helpful. Can you advise if there is any L series MCU that supports flash swap? Thanks Tuo
You are welcome.
Unfortunately none of the L series support flash swap.
Regards!
Jorge Gonzalez
Thank you Jorge!