Does K70 fully support the EMV spec ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does K70 fully support the EMV spec ?

跳至解决方案
1,041 次查看
youjongan
Contributor I

Dear Community..

Currently, i use the K70 MCU in my project and use the UART0 to control the IC card.

I want to know that K70 is fully supported on EMV spec (Level 1).

if the K70 is any limitations in order to pass EMV certification, please share the detailed information about it. 

Specially, on ISO7816 T=1 mode, Does it possible to support  the 11 etu ?

(11 etu should be support in order to pass EMV. )

if not supported, please tell me any solution.

Thanks

Yoo.

标签 (1)
0 项奖励
回复
1 解答
946 次查看
miduo
NXP Employee
NXP Employee

Hi, Yoo

Yes, the K70 really support  ISO7816(EMV Lv1). And unfortunately it does not support 11 etu.

在原帖中查看解决方案

0 项奖励
回复
1 回复
947 次查看
miduo
NXP Employee
NXP Employee

Hi, Yoo

Yes, the K70 really support  ISO7816(EMV Lv1). And unfortunately it does not support 11 etu.

0 项奖励
回复