Do I need to use the PCS0 pin to activate the SPI in slave mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Do I need to use the PCS0 pin to activate the SPI in slave mode?

1,066 次查看
marcohess
Contributor II

I am using a K22FN on a custom board where I am interfacing SPI1 in slave mode to some SPI 'like' master device.

This device does not generate a chip select signal. Instead it uses two I/O signals. One to signal the start of a new cycle and one to signal the start of new 16 bit word transfer after which the clock starts for the data transfer.

As such I had not connected the PCS0 input and instead configured that pin as a general I/O.

However, I can't seem to get my device to transmit anything in slave mode.

Does the PCS0 need to be used? Or can I set it to enabled in software? If not, can I tie the pin to a fixed level?

0 项奖励
回复
1 回复

925 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Marco,

I guess that you must use the PCS0/SS pin when you want the K22 works as slave device.

In Slave mode, the SPI module respons to externally controlled serial transfer. The SCK signal and the PCS0/SS signals are configured as input and driven by an SPI bus master.

Wish it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复