Hello!
I have a custom board where I need both NMI and reset pin.
I use KDS 3.0.0 and I am not using processorexpert. Debugger is Jlink. Everything else is working fine as long as these pins stays inactive.
I tried the following code in an header file:
typedef struct stKINETIS_FLASH_CONFIGURATION | // loaded from FLASH 0x00000400 at reset |
{
unsigned char ucBackdoorComparisonKey[8];
unsigned char ucProgramFlashProtection[4];
unsigned char reserved1;
unsigned char reserved2;
unsigned char ucNonvolatileOption;
unsigned char ucDataFlashSecurity;
} KINETIS_FLASH_CONFIGURATION;
const KINETIS_FLASH_CONFIGURATION __attribute__((section(".f_config"))) __flash_config
= {
0xff,0xff,0xff,0xff, 0xff,0xff,0xff,0xff,
0xff,0xff,0xff,0xff, | |
0xff, | |
0xff, | |
0b11110011, //disable nmi and reset | |
0b11111110 //unsecure |
};
This does not seem to have any effect, reading memory location 0x040D gives 0xFF and pins are still active.
Is there something that owerrides this or what have I missed?
Best regards
Magnus Lundell
Finland
Solved! Go to Solution.
Hi Magnus Lundell,
I think you modify the wrong address, because from your defination:
const KINETIS_FLASH_CONFIGURATION __attribute__((section(".f_config"))) __flash_config
= {
0xff,0xff,0xff,0xff, 0xff,0xff,0xff,0xff,
0xff,0xff,0xff,0xff, | |
0xff, | |
0xff, | |
0b11110011, //disable nmi and reset | |
0b11111110 //unsecure |
};
Do you mean your .f_config is from 0x400? then your 0b11110011, //disable nmi and reset actually is 0X40E, not 0x40D, please take care!
I create a barebone KDS project, I can modify the 0X40D successfully!
The attachment is my test project, you can refer to it!
After you modify it, you can generate a .hex file to check your 0X40D, whether you have modified it successfully!
Wish it helps you!
If you still have question, please contact me!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Magnus Lundell,
I think you modify the wrong address, because from your defination:
const KINETIS_FLASH_CONFIGURATION __attribute__((section(".f_config"))) __flash_config
= {
0xff,0xff,0xff,0xff, 0xff,0xff,0xff,0xff,
0xff,0xff,0xff,0xff, | |
0xff, | |
0xff, | |
0b11110011, //disable nmi and reset | |
0b11111110 //unsecure |
};
Do you mean your .f_config is from 0x400? then your 0b11110011, //disable nmi and reset actually is 0X40E, not 0x40D, please take care!
I create a barebone KDS project, I can modify the 0X40D successfully!
The attachment is my test project, you can refer to it!
After you modify it, you can generate a .hex file to check your 0X40D, whether you have modified it successfully!
Wish it helps you!
If you still have question, please contact me!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for your time!
Now the problem is solved, and I can say that I should have observed that lines :smileyhappy: ,
/* Flash Configuration */
.section .FlashConfig, "a"
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xFFFFFFFE
,in the startupfile.s file the first time.
You are right about my mistake with the adress too.
Thank you!