Difference between MKW36Z512xxx and MKW36A512xxx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between MKW36Z512xxx and MKW36A512xxx

869 Views
rajasekhar_99
Contributor I

If one has to port from MKW36Z to MKW36A, what are the things that one has to take care of?

I have checked data sheets of both of them, they have same specifications.

I have checked NXP forum, it says the only difference is MKW36A being AEC Q100 grade-2 qualified, and MKW36Z being industrail grade.

 Are these the only difference?

 

0 Kudos
Reply
2 Replies

866 Views
nxf56274
NXP Employee
NXP Employee

Hi,

If you concern on the code function, both mcu has no difference.

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

856 Views
rajasekhar_99
Contributor I

Thank you my concern is about code migration only. But I did not understand, this difference in thermal grading, both of them seem to work in same ambient temperature (from -40 to 105 as said in datasheets of both). 

0 Kudos
Reply