Difference between MK11DN512AVLK5 & MK11DN512VLK5 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between MK11DN512AVLK5 & MK11DN512VLK5 ?

1,905 Views
eduardrazumovsk
Contributor III

Hello,

What is the difference between MK11DN512AVLK5 & MK11DN512VLK5 ?

Thanks & Regards,

Eduard

0 Kudos
Reply
3 Replies

1,785 Views
DerekLau
Contributor IV

MK11DN512AVLK5

CaptureA.JPG.jpg


MK11DN512VLK5

Capture.JPG.jpg

0 Kudos
Reply

1,785 Views
eduardrazumovsk
Contributor III

Hi,

Thanks for the answer

Is this the only difference ?

Regardless the supply current, i can use each ? they are pin compatible ?

Thanks

Eduard

0 Kudos
Reply

1,785 Views
PatriciaTeran
Contributor III

Hi, Eduard

There are a few differences, but in general they are pretty much the same, and yes they are pin compatible.

You can download a document at this link so you can review all the differences.

http://cache.freescale.com/files/microcontrollers/doc/eng_bulletin/EB800.pdf?fasp=1&WT_TYPE=Engineer...

Hope it helps.

Best regards!

Patricia

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply