Deviation in Board Power Supply (V_BRD) & AFE Channels

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Deviation in Board Power Supply (V_BRD) & AFE Channels

843 Views
RushinMehta
Contributor I

Hello All,

I have 3 Dev-kits (TWR-KM35Z7M), in all of them the V_BRD power net which is said to be 3.3V [Both in SCH & in the datasheet of the IC used NCP1117ST33T3G (U2)] is measured to be 4.1V.

Even in the BRD file, the net says P3V3. But our Test equipment show it to be 4.1V.

RushinMehta_0-1688369611565.png

So, can this cause any issues in the AFE Channels & their Voltage references as they are connected directly?

We are developing an Energy Meter & we are facing an issue that when I give a Sine wave to AFE Channel 0 & another phase shifted sine wave to AFE Channel 1,channel 0 saturates, even if the pk-pk is below 400mV (500mV is the range of AFE channels). 

Also when we give the same waveform for AFE Channel 2, it does not saturate !

Is this due to improper Voltage reference or is this something else? 

 

 

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

797 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @RushinMehta,

Just for double check, this behavior happens only on AFE Channel 0?

Have you tried using the SDK's examples configuration for AFE Channel 0? You could use the afe_interrupt example configuration and test the behavior of the AFE Channel 0.

Finally, could you please try reducing the voltage of the sine wave? Does it stop saturating with any pk-pk voltage? 

Best regards, Raul.

0 Kudos
Reply