Debugging issues with different versions of MK60FN1M0VLQ155 materials 3N96B and 5N96B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging issues with different versions of MK60FN1M0VLQ155 materials 3N96B and 5N96B

1,491 Views
Alan7
Contributor I

MK60FN1M0VLQ15 material 3N96B and 5N96B have different versions, and the current network port pin does not work. It is OK to replace them with 3N96B. Please help and support me to see the differences between the two versions and see how to modify them. Thank you!

0 Kudos
Reply
5 Replies

1,477 Views
vicentegomez
NXP TechSupport
NXP TechSupport

The only difference is that mask set 5N96B and mask set 3N96B has different errata sheet, but you can find both errata sheets on the next link

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

 

I hope this will help you.

 

 

0 Kudos
Reply

1,472 Views
Alan7
Contributor I

There is no difference between the 5N96B and 3N96B errata comparisons, and the network interface link is not available. What troubleshooting needs to be done?

0 Kudos
Reply

1,447 Views
vicentegomez
NXP TechSupport
NXP TechSupport

 You can check if you have any data on the ethernet pins, please check that you do not have any manufacture problem, like open pin, solder short, missing part, wrong part.

 

All the other functions are working? 

Regards

 

0 Kudos
Reply

1,440 Views
Alan7
Contributor I

The 3N96B version is tested as Pass, and the 5N96B version is tested as Fail,Can be ruled out as a welding problem,What is the difference between the two versions?

0 Kudos
Reply

1,396 Views
vicentegomez
NXP TechSupport
NXP TechSupport

the only differences are the mask set. Only the errata are different

Regards

 

0 Kudos
Reply