Debouncing time in TSS3.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Debouncing time in TSS3.1

跳至解决方案
1,410 次查看
sureshjaggal
Contributor III

Dear Folks,

I am using TSS3.1 in TSI configuration and KL05Z32 to develop a HMI application.

It is mentioned in the TSS application reference manual that the debouncing time  for the touch Input is taken care by the TSS library .

My questions are

1) How much is the debouncing time , that the TSS is configured with ?

2) How can we change the debouncing time for our requirements in TSS ?

Thanks & Regards,

Suresh Jaggal. 

标记 (2)
1 解答
1,330 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Suresh

The debouncing rate is modified with the ResponseTime register that defines how many samples need to be valid before considering a measured value as valid. The feature is available in all key detector versions. Refer to the TSS reference manual - Number of samples register.

Depending your application maybe you need more or less samples for your application.

I hoe this will help you.

Regards

Vicente.

在原帖中查看解决方案

1 回复
1,331 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Suresh

The debouncing rate is modified with the ResponseTime register that defines how many samples need to be valid before considering a measured value as valid. The feature is available in all key detector versions. Refer to the TSS reference manual - Number of samples register.

Depending your application maybe you need more or less samples for your application.

I hoe this will help you.

Regards

Vicente.