Deadtime insertion on FTM2 with FRDM-KE06Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Deadtime insertion on FTM2 with FRDM-KE06Z

Jump to solution
664 Views
brunotremblay
Contributor III

Hi,

I'm trying to the FTM2 channels 0 to 3 to generate Phase-shift PWM signal with the FRMD-KE06Z board as explained in the appnote "AN5142 Features of the FlexTimer Module" in the section 3.4. For generating Phase-shift signals there is no problem. It's easy to change the amount of phase-shift. However, I don't see any deadtime between the complementary channels CH0 and CH1 or CH2 and CH3. The only changes I made from AN5142 is using SIM_SCGC instead of SIM_SCGC6 to enable FTM2 module clock and changing FTM0_ for FTM2_.

I tried to change the value in the FTM2_DEADTIME register, but at the scope screen's there's no deadtime.

Here is the values of the registers:

SIM_SCGC          0x00003080

FTM2_SC             0x00000010

FTM2_MOD          0x000003E8

FTM2_C0SC         0x00000008

FTM2_C0V            0x0000000A

FTM2_C1SC         0x00000008

FTM2_C1V            0x000001FE

FTM2_C2SC         0x00000008

FTM2_C2V            0x000000FA

FTM2_C3SC         0x00000008

FTM2_C3V            0x000002EE

FTM2_MODE        0x00000005

FTM2_COMBINE  0x00001313

FTM2_DEADTIME 0x0000001E

Any suggestions?

Best Regards,

Bruno

Labels (1)
0 Kudos
1 Solution
448 Views
brunotremblay
Contributor III

Hi,

Found the problem. Deadtime insertion doesn't work when fixed frequency clock is selected instead of system clock.

Best Regards,

Bruno

View solution in original post

0 Kudos
1 Reply
449 Views
brunotremblay
Contributor III

Hi,

Found the problem. Deadtime insertion doesn't work when fixed frequency clock is selected instead of system clock.

Best Regards,

Bruno

0 Kudos