Hi estephania_martinez,
I configured KW36 DTM as mentioned in the below link (Through a 2-wire UART interface)
Direct Test Mode (DTM) Configurations for the KW family
But to verify the DTM behavior I tested using the below commands
1. LE Reset
(a) 0x0000
(b) 0x0204
(c) 0x0300
2. LE Transmitter Test
0x8000
3. LE Receiver Test
0x4000
4. LE Test End
0xC000
In the above-mentioned commands, LE Reset is not getting passed with all the 3 commands and LE Test End command is also failed.
Can you please check this issue?
Hardware used: USB to TTL converter (3.3v logic level)
Thanks!
Regards,
Naven Suresh
Hello,
Are you using test tool? Could you please share with me the complete command you sent and the response ?
Regards,
Estephania