DTM configuration for KW36

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DTM configuration for KW36

1,842 次查看
nsuresh2
Contributor III

Hi estephania_martinez‌,

I configured KW36 DTM as mentioned in the below link (Through a 2-wire UART interface)

Direct Test Mode (DTM) Configurations for the KW family 

But to verify the DTM behavior I tested using the below commands

1. LE Reset 

    (a)  0x0000

    (b)  0x0204

    (c)  0x0300

2. LE Transmitter Test

      0x8000

3. LE Receiver Test

      0x4000

4. LE Test End

      0xC000

In the above-mentioned commands, LE Reset is not getting passed with all the 3 commands and LE Test End command is also failed.

Can you please check this issue?

Hardware used: USB to TTL converter (3.3v logic level)

Thanks!

Regards,

Naven Suresh

标记 (2)
0 项奖励
回复
2 回复数

1,708 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Are you using test tool? Could you please share with me the complete command you sent and the response ?

Regards,

Estephania

0 项奖励
回复

1,708 次查看
nsuresh2
Contributor III

Hi,

Thanks for the response.

It is not the test tool. It is a third-party tool and now it is working fine the issue was in address configuration.

Thanks!

Regards,

Naven Suresh

0 项奖励
回复