DSPI slave example on FRDM-K66F like board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DSPI slave example on FRDM-K66F like board

跳至解决方案
1,481 次查看
mdecandia
Contributor III

Hi all,

we are testing the dspi samples from SDK and they are not working on a board derived from FRDM-K66F.  There are few changes (clock frequencies, pinmuxing) but they should not impact SPI slave functionality.

Do they  should work on this evb?

 

Michele

0 项奖励
回复
1 解答
1,442 次查看
mdecandia
Contributor III

Hi @RaRo,

thanks for your feedback. In the meanwhile we have found the issue: we were using the SPI0_PCS5 as chip select pin that cannot be used as SPI slave.

Kind regards.

Michele

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,443 次查看
mdecandia
Contributor III

Hi @RaRo,

thanks for your feedback. In the meanwhile we have found the issue: we were using the SPI0_PCS5 as chip select pin that cannot be used as SPI slave.

Kind regards.

Michele

 

0 项奖励
回复
1,446 次查看
RaRo
NXP TechSupport
NXP TechSupport

Hello @mdecandia,

Could you please help us with more information related with your issue? Did you receive an error while debugging or your problem is that the communication is not working? Could you tell us which other changes did you make in your board? What clock frequency are you working with? What pins do you configure for the DSPI you are working with? Which SDK example and version are you using?

Best regards, Raul.

0 项奖励
回复