DMAMUX_CHCFGn

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMAMUX_CHCFGn

1,839件の閲覧回数
JBM
Contributor V

I'm looking for the DMA Channel Sources for the K22FN512VLH12 (Freedom K22 Board processor), but can't find them.  These are the values written to the DMAMUX_CHCFGn registers.  The reference manual says to see the chip specific documentation.  The data sheet for this chip (see data sheet) doesn't seem to have it.

I'm using KDS 3.0 and the include file, MK22F51212.h doesn't have them either.  

Any ideas?

Thanks.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,771件の閲覧回数
mjbcswitzerland
Specialist V

Hi

DMA sources are always in the user's manual - for the K22FN512:

pastedImage_1.png

This are the DMAMUX0 trigger defines from the uTasker project (when K22FN512 is used); I don't think that the NXP references support portable DMA usage and so the values probably need to be looked up and hard coded for each processor type that will be used.

          #define DMAMUX0_CHCFG_SOURCE_UART0_RX      2                   // 0x02 UART0 RX - DMAMUX_CHCFG_xx are available on DMA MUX 0 and on DMA MUX 1 (when available)
          #define DMAMUX0_CHCFG_SOURCE_UART0_TX      3                   // 0x03 UART0 TX
          #define DMAMUX0_CHCFG_SOURCE_UART1_RX      4                   // 0x04 UART1 RX
          #define DMAMUX0_CHCFG_SOURCE_UART1_TX      5                   // 0x05 UART1 TX
          #define DMAMUX0_CHCFG_SOURCE_UART2_RX      6                   // 0x06 UART2 RX
          #define DMAMUX0_CHCFG_SOURCE_UART2_TX      7                   // 0x07 UART2 TX
          #define DMAMUX0_CHCFG_SOURCE_UART3_RX      8                   // 0x08 UART3 RX
          #define DMAMUX0_CHCFG_SOURCE_UART3_TX      9                   // 0x09 UART3 TX
              #define DMAMUX0_CHCFG_SOURCE_UART4_RX  10                  // 0x0a UART4 RX
              #define DMAMUX0_CHCFG_SOURCE_UART4_TX  11                  // 0x0b UART4 TX
              #define DMAMUX0_CHCFG_SOURCE_UART5_RX  12                  // 0x0c UART5 RX
              #define DMAMUX0_CHCFG_SOURCE_UART5_TX  13                  // 0x0d UART5 TX
              #define DMAMUX0_CHCFG_SOURCE_I2S0_RX   14                  // 0x0e I2S0 RX
              #define DMAMUX0_CHCFG_SOURCE_I2S0_TX   15                  // 0x0f I2S0 TX
              #define DMAMUX0_CHCFG_SOURCE_SPI0_RX   16                  // 0x10 SPI0 RX
              #define DMAMUX0_CHCFG_SOURCE_SPI0_TX   17                  // 0x11 SPI0 TX
              #define DMAMUX0_CHCFG_SOURCE_SPI1_RX   18                  // 0x12 SPI1 RX
              #define DMAMUX0_CHCFG_SOURCE_SPI1_TX   19                  // 0x13 SPI1 TX
              #define DMAMUX0_CHCFG_SOURCE_SPI2_RX   20                  // 0x14 SPI2 RX
              #define DMAMUX0_CHCFG_SOURCE_SPI2_TX   21                  // 0x15 SPI2 TX
              #define DMAMUX0_CHCFG_SOURCE_I2C0      22                  // 0x16 I2C0 - DMAMUX0_CHCFG_xx are only available on DMA MUX 0
              #define DMAMUX0_CHCFG_SOURCE_I2C1_2    23                  // 0x17 I2C1 (or I2C2)
          #define DMAMUX0_CHCFG_SOURCE_FTM0_C0       24                  // 0x18 FTM0/TPM0 channel 0
          #define DMAMUX0_CHCFG_SOURCE_FTM0_C1       25                  // 0x19 FTM0/TPM0 channel 1
          #define DMAMUX0_CHCFG_SOURCE_FTM0_C2       26                  // 0x1a FTM0/TPM0 channel 2
          #define DMAMUX0_CHCFG_SOURCE_FTM0_C3       27                  // 0x1b FTM0/TPM0 channel 3
          #define DMAMUX0_CHCFG_SOURCE_FTM0_C4       28                  // 0x1c FTM0/TPM0 channel 4
          #define DMAMUX0_CHCFG_SOURCE_FTM0_C5       29                  // 0x1d FTM0/TPM0 channel 5
          #define DMAMUX0_CHCFG_SOURCE_FTM0_C6       30                  // 0x1e FTM0/TPM0 channel 6
          #define DMAMUX0_CHCFG_SOURCE_FTM0_C7       31                  // 0x1f FTM0/TPM0 channel 7
          #define DMAMUX0_CHCFG_SOURCE_FTM1_C0       32                  // 0x20 FTM1/TPM1 channel 0
          #define DMAMUX0_CHCFG_SOURCE_FTM1_C1       33                  // 0x21 FTM1/TPM1 channel 1
              #define DMAMUX0_CHCFG_SOURCE_FTM2_C0       34              // 0x22 FTM2/TPM2 channel 0
              #define DMAMUX0_CHCFG_SOURCE_FTM2_C1       35              // 0x23 FTM2/TPM2 channel 1
              #define DMAMUX0_CHCFG_SOURCE_IEEE1588_T0   36              // 0x24 IEEE 1588 timer 0 (alternative)
              #define DMAMUX0_CHCFG_SOURCE_FTM3_C1       36              // 0x24 FTM3 channel 1
              #define DMAMUX0_CHCFG_SOURCE_IEEE1588_T1   37              // 0x25 IEEE 1588 timer 1 (alternative)
              #define DMAMUX0_CHCFG_SOURCE_FTM3_C2       37              // 0x25 FTM3 channel 2
              #define DMAMUX0_CHCFG_SOURCE_IEEE1588_T2   38              // 0x26 IEEE 1588 timer 2 (alternative)
              #define DMAMUX0_CHCFG_SOURCE_FTM3_C3       38              // 0x26 FTM3 channel 3
              #define DMAMUX0_CHCFG_SOURCE_IEEE1588_T3   39              // 0x27 IEEE 1588 timer 3 (alternative)
          #define DMAMUX0_CHCFG_SOURCE_ADC0          40                  // 0x28 ADC0
                  #define DMAMUX0_CHCFG_SOURCE_ADC1  41                  // 0x29 ADC1
              #define DMAMUX0_CHCFG_SOURCE_CMP0      42                  // 0x2a CMP0
              #define DMAMUX0_CHCFG_SOURCE_CMP1      43                  // 0x2b CMP1
              #define DMAMUX0_CHCFG_SOURCE_DAC0      45                  // 0x2d DAC0
                  #define DMAMUX0_CHCFG_SOURCE_CMT   47                  // 0x2f CMT
              #define DMAMUX0_CHCFG_SOURCE_PDB0      48                  // 0x30 PDB 0
          #define DMAMUX0_CHCFG_SOURCE_PORTA         49                  // 0x31 port A
          #define DMAMUX0_CHCFG_SOURCE_PORTB         50                  // 0x32 port B
          #define DMAMUX0_CHCFG_SOURCE_PORTC         51                  // 0x33 port C
          #define DMAMUX0_CHCFG_SOURCE_PORTD         52                  // 0x34 port D
          #define DMAMUX0_CHCFG_SOURCE_PORTE         53                  // 0x35 port E
          #define DMAMUX0_CHCFG_SOURCE_FTM3_C4       54                  // 0x36 FTM3 channel 4
          #define DMAMUX0_CHCFG_SOURCE_FTM3_C5       55                  // 0x37 FTM3 channel 5
          #define DMAMUX0_CHCFG_SOURCE_FTM3_C6       56                  // 0x38 FTM3 channel 6
          #define DMAMUX0_CHCFG_SOURCE_FTM3_C7       57                  // 0x39 FTM3 channel 7
              #define DMAMUX0_CHCFG_SOURCE_DMAMUX0   (58 | DMAMUX_CHCFG_TRIG) // 0x3a DMA MUX - always enabled
              #define DMAMUX0_CHCFG_SOURCE_DMAMUX1   (59 | DMAMUX_CHCFG_TRIG) // 0x3b DMA MUX - always enabled
              #define DMAMUX0_CHCFG_SOURCE_DMAMUX2   (60 | DMAMUX_CHCFG_TRIG) // 0x3c DMA MUX - always enabled
              #define DMAMUX0_CHCFG_SOURCE_DMAMUX3   (61 | DMAMUX_CHCFG_TRIG) // 0x3d DMA MUX - always enabled
              #define DMAMUX0_CHCFG_SOURCE_DMAMUX4   (62 | DMAMUX_CHCFG_TRIG) // 0x3e DMA MUX - always enabled
              #define DMAMUX0_CHCFG_SOURCE_DMAMUX5   (63 | DMAMUX_CHCFG_TRIG) // 0x3f DMA MUX - always enabled

      #define DMAMUX0_DMA0_CHCFG_SOURCE_PIT0     (DMAMUX0_CHCFG_SOURCE_DMAMUX0)
        #define DMAMUX0_DMA0_CHCFG_SOURCE_PIT1   (DMAMUX0_CHCFG_SOURCE_DMAMUX1)
        #define DMAMUX0_DMA0_CHCFG_SOURCE_PIT2   (DMAMUX0_CHCFG_SOURCE_DMAMUX2)
        #define DMAMUX0_DMA0_CHCFG_SOURCE_PIT3   (DMAMUX0_CHCFG_SOURCE_DMAMUX3)

Regards

Mark


Complete Kinetis solutions for professional needs, training and support: http://www.utasker.com/kinetis.html
Kinetis K22:
- http://www.utasker.com/kinetis/FRDM-K22F.html
- http://www.utasker.com/kinetis/TWR-K22F120M.html
- http://www.utasker.com/kinetis/BLAZE_K22.html
- http://www.utasker.com/kinetis/tinyK22.html
uTasker: supporting >1'000 registered Kinetis users get products faster and cheaper to market
Request Free emergency remote desk-top consulting at http://www.utasker.com/services.html

Open Source version at https://github.com/uTasker/uTasker-Kinetis

0 件の賞賛
返信

1,771件の閲覧回数
JBM
Contributor V

Thanks for posting these.  It's a lot of help.

0 件の賞賛
返信