Here is what I achieved so far with channel linking:
* DMA will transfer out ADC results: 2-ADC channels(c1,c2), 3 samples per channel (s1,s1,s3)
----------------------------------------------------------------------------------------------------------------------------------
...
DMA0->TCD[0].SADDR = (uint32_t)&adc_mux[0]; // (adc_mux[] = {c1, c2} //channel-1, 2
DMA0->TCD[0].DADDR = (uint32_t)&ADC1->SC1[0];
...
-----------------------------------------------------------------------------------------------------------------------------------
DMA0->TCD[1].SADDR = (uint32_t) &ADC1->R[0];
DMA0->TCD[1].DADDR = (uint32_t)&adc_result[0];
DMA0->TCD[1].SOFF = 0x00;
//**** 16 bit => 2 bytes
DMA0->TCD[1].DOFF = 0x02;
DMA0->TCD[1].ATTR = DMA_ATTR_SSIZE(1)| DMA_ATTR_DSIZE(1);
DMA0->TCD[1].NBYTES_MLNO = 0x02;
DMA0->TCD[1].CITER_ELINKNO = (DMA_CITER_ELINKNO_ELINK_MASK | 0x06);
DMA0->TCD[1].BITER_ELINKNO =(DMA_BITER_ELINKNO_ELINK_MASK|0x0000|0x06);
DMA0->TCD[1].SLAST = 0x00;
DMA0->TCD[1].DLAST_SGA = -12;
DMA0->TCD[1].CSR = DMA_CSR_INTMAJOR_MASK |DMA_CSR_MAJORELINK_MASK | DMA_CSR_MAJORLINKCH(0);
------------------------------------------------------------------------------------------------------------------------------
* adc_result[ ]: [ c1s1, c2s1, c1s2, c2s2, c1s3, c2s3 ] and repeat -------------- so far so good!
Now I want to change outputs to be:
* adc_result[ ]: [ c1s1, c1s2, c1s3, c2s1, c2s2, c2s3 ] and repeat
* (Attention: ADC still produce results in order of: c1s1, c2s1, c1s2, c2s2, c1s3, c2s3 )!
* How can I achieve this?
Thanks!
Jerry
已解决! 转到解答。
Hi Jerry Lian
It is not possible to set that order with a configuration of DOFF, CITER, BITER, etc. for this case you could use another DMA to order your array, but this is not the most optimal implementation, so I don't know if it works for you. Another option is to use scatter gatter feature, but for this you will have to implement 12 different TCD configuration, so I don't know if it works for you.
Hope this information could help you. Please let me know fi you have any other question.
Best Regards
Jorge Alcala
Hi Jerry Lian
It is not possible to set that order with a configuration of DOFF, CITER, BITER, etc. for this case you could use another DMA to order your array, but this is not the most optimal implementation, so I don't know if it works for you. Another option is to use scatter gatter feature, but for this you will have to implement 12 different TCD configuration, so I don't know if it works for you.
Hope this information could help you. Please let me know fi you have any other question.
Best Regards
Jorge Alcala
Hi, Jorge:
I have figured it by using dynamic scatter/gather feature. And I just need one TCD instead of 12 in TCD-loop, surely I need to update TCD during major interrupt!
Thanks for your answer!
Jerry