Crc computation on K24 chip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Crc computation on K24 chip

1,486件の閲覧回数
June
Contributor I

Hi,

I'm performing crc computation on K24 chip during run-time. As the address range to compute the crc is quite huge, it is broken up into several cycles. How to have the chip start a new calculation using an intermediate crc value from the previous calculation?

For example:

cycle 1: crc1 = Calculated crc from address 0x0001 to 0x0020

cycle 2: crc2 = calculated crc from crc1 and address 0x0021 to 0x0040

and so on...

How should crc1 be parsed in during cycle 2? As seed value or as a data?

Here's my code but it doesn't work:

<code>

static uint32_t Crc32(uint32_t const * const pData, uint32_t numLongs, uint32_t initCrc)

{

   // Steps #1 and #2

   CRC_CTRL = (CRC_CTRL_TOT(2U)) | // Input bits & bytes are transposed

   (CRC_CTRL_TOTR(2U)) | // Output bits & bytes are transposed

   (0UL << CRC_CTRL_WAS_SHIFT) | // Ready to write data

   (1UL << CRC_CTRL_TCRC_SHIFT); // 32-bit CRC

   // Step #3

   CRC_GPOLY = 0x04C11DB7; // CRC32 polynomial

   // Step #4 - Indicate seed will be written

   CRC_CTRL = (CRC_CTRL_TOT(2U)) | // Input bits & bytes are transposed

   (CRC_CTRL_TOTR(2U)) | // Output bits & bytes are transposed

   (1UL << CRC_CTRL_WAS_SHIFT) | // Ready to write seed

   (1UL << CRC_CTRL_TCRC_SHIFT); // 32-bit CRC

   // Step #5 - Write seed

  CRC_DATA = initCrc;

   // Step #6 - Indicate that data follows

   CRC_CTRL = (CRC_CTRL_TOT(2U)) | // Input bits & bytes are transposed

   (CRC_CTRL_TOTR(2U)) | // Output bits & bytes are transposed

   (0UL << CRC_CTRL_WAS_SHIFT) | // Ready to write data

   (1UL << CRC_CTRL_TCRC_SHIFT); // 32-bit CRC

   // Step #7 - Write the data values.

   for (uint32_t i = 0; i < numLongs; i++)

  {

    CRC_DATA = pData[i];

  }

   // Step #8 - Return CRC result.

   return CRC_DATA;

}

  

// Note: the following is a pseudo code just to illustrate the logic

// The following doesn't work. What's wrong?

main()

{

  while (!crcDone)

  {

     readData(&data[0]);

     if (cycle1)

     {

       crc = crc32(data[0], numBytes, 0xFFFFFFFFUL);

     }

     else

     {

       crc = crc32(data[0], numBytes, crc);

     }

  }

  CompareCrcWithStoredCrc();

}

// I have also tried the following but it doesn't work either:

main()

{

  while (!crcDone)

  {

     readData(&data[4]);

     if (cycle1)

     {

       crc = crc32(data[4], numBytes, 0x0UL);

     }

     else

     {

       memcpy(&data[0], &crc, 4);

       crc = crc32(data[0], numBytes+4, 0x0UL);

     }

  }

  CompareCrcWithStoredCrc();

}

<code>

Appreciate some advice. Thanks!

0 件の賞賛
返信
3 返答(返信)

1,398件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi,

Comparing your code with the SDK example I see that your missing the clock enable for the CRC module.

I will suggest to check the example code that is in the MK24 SDK. You can download it from here:

https://mcuxpresso.nxp.com/

Let me know if this helps you.

Best Regards,

Alexis Andalon

0 件の賞賛
返信

1,398件の閲覧回数
June
Contributor I

Hi Alexis,

The SCGC clock for CRC is already enabled in the startup code and i have checked that it is set for crc. So unfortunately it doesn't help. Thanks. 

I'm curious to know if anyone has had any success using the crc this way?

0 件の賞賛
返信

1,398件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi YiJun,

I found something strange in the previous code.

The function static uint32_t Crc32(uint32_t const * const pData, uint32_t numLongs, uint32_t initCrc) receive a pointer for the data but when you call the function you only use the value from the array data[0] or data[4]. I think if you store the data in the array you should pass the direction from the first pointer (data or &data[0]).

Also, I will suggest to test the SDK example, maybe you could base your application in this one.

Let me know if this helps you.

Best Regards,

Alexis Andalon

0 件の賞賛
返信