Coverity issues for KW36 SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Coverity issues for KW36 SDK

5,583 Views
nsuresh2
Contributor III

Hi,

I have run the coverity for KW36 SDK and I have found 555 issues.

Please find the attached coverity report.

Let us know when these issues can be fixed? 

Thanks!

Regards,

Naven Suresh 

Labels (1)
Tags (3)
10 Replies

5,138 Views
xing_chang
NXP Employee
NXP Employee

Hi nsuresh2@visteon.com‌,

Version of Coverity?

Aggressivity Level?

0 Kudos
Reply

5,138 Views
nsuresh2
Contributor III

Hi XingChang‌,

Version of Coverity: 2018.06-11

Aggressivity Level: High

Regards,

Naven Suresh.

0 Kudos
Reply

5,138 Views
xing_chang
NXP Employee
NXP Employee

Hi Naven,

We run coverity with -agresivity level low.
Also coverity are providing "false positive findings" that in our system are marked as resolved.

0 Kudos
Reply

5,138 Views
nsuresh2
Contributor III

Hi XingChang‌,

The Coverity has been run already and the report is shared.

Is the Coverity results run by you are matching with our report?

If necessary, Can you run the Coverity with high aggressive level and check?

Regards,

Naven Suresh

0 Kudos
Reply

5,138 Views
xing_chang
NXP Employee
NXP Employee

Hi Naven,

Could you please tell me, which project did you run Coverity on? I have run on ble_shell freertos and I only obtain ~270 total defects, while in the excel file there are ~550. And also could you please tell me how you have configured the analysis? (a screenshot of the Analysis Options pop-up window would be helpful)

0 Kudos
Reply

5,138 Views
nsuresh2
Contributor III

Hi XingChang‌,

We are running Coverity for Wireless_Uart BLE (FreeRTOS) project along with our application.

And the configuration settings are shared through the mail.

Thanks!

Regards,

Naven Suresh

0 Kudos
Reply

5,138 Views
xing_chang
NXP Employee
NXP Employee

Hi Naven,

We try to run it according to your settings. Can you run it according to our settings?

0 Kudos
Reply

5,138 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Let me check about this, whenever I get an update I'll let you know.

Regards,

Estephania

0 Kudos
Reply

5,138 Views
xing_chang
NXP Employee
NXP Employee

Hi estephania_martinez‌,

Is there any update? 

0 Kudos
Reply

5,138 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

No update yet, we are currently waiting for an official answer on this. Sorry for the inconveniences

0 Kudos
Reply