Could I set OSCERCLK as the PWM clock source in FTM moudle in FRDM-K64F?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Could I set OSCERCLK as the PWM clock source in FTM moudle in FRDM-K64F?

1,142 次查看
gloria
Contributor III

Hi, could I set OSCERCLK as the PWM clock source in FTM moudle in FRDM-K64F? If yes, how could I do it? Many thanks!

标签 (1)
0 项奖励
回复
1 回复

922 次查看
mjbcswitzerland
Specialist V

Hi

The FTM (used for PWM) can be optionally clocked from the MCGFFCLK but not directly from OSCERCLK.

See µTasker MCG Configuration Support

Depending on the configuration of the MCG ,MCGFFCLK may be related to OSCERCLK (or derived from it) but it is highly unlikely that it will be the same frequency.

Regards

Mark

Kinetis: µTasker Kinetis support

K64: µTasker Kinetis FRDM-K64F support  / µTasker Kinetis TWR-K64F120M support  / µTasker Kinetis TWR-K65F180M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 项奖励
回复