Correct setup of the K10 Internal Reference Clock...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Correct setup of the K10 Internal Reference Clock...

3,300 Views
Alex_HMBE
Contributor II

We're trying to get the full 72MHz system clock out of a 64-pin, 72MHz K10. We've pulled code in from PE, setting the DCO up to give us 2197x32.768=71.99MHz. After setting up a UART and noticing some bad characters, I checked the bit period on a scope and found that it was off by 2.9% (after taking the baud rate error created by the UART divisor into account).

So, my question is - should the FLL output, using the IRC, be able to produce a reliable 72MHz?

Here's the setup code from PE:

void __init_hardware()

{

  /*** PE initialization code after reset ***/

  SCB_VTOR = (uint32_t)__vector_table; /* Set the interrupt vector table position */

  /* Disable the WDOG module */

  /* WDOG_UNLOCK: WDOGUNLOCK=0xC520 */

  WDOG_UNLOCK = (uint16_t)0xC520U;     /* Key 1 */

  /* WDOG_UNLOCK : WDOGUNLOCK=0xD928 */

  WDOG_UNLOCK  = (uint16_t)0xD928U;    /* Key 2 */

  /* WDOG_STCTRLH: ??=0,DISTESTWDOG=0,BYTESEL=0,TESTSEL=0,TESTWDOG=0,??=0,??=1,WAITEN=1,STOPEN=1,DBGEN=0,ALLOWUPDATE=1,WINEN=0,IRQRSTEN=0,CLKSRC=1,WDOGEN=0 */

  WDOG_STCTRLH = (uint16_t)0x01D2U;                 

  /* System clock initialization */

  /* SIM_SCGC5: PORTA=1 */

  SIM_SCGC5 |= (uint32_t)0x0200UL;     /* Enable clock gate for ports to enable pin routing */

  /* SIM_CLKDIV1: OUTDIV1=0,OUTDIV2=1,OUTDIV3=3,OUTDIV4=3,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  SIM_CLKDIV1 = (uint32_t)0x01330000UL; /* Update system prescalers */

  /* SIM_SOPT2: PLLFLLSEL=0 */

  SIM_SOPT2 &= (uint32_t)~0x00010000UL; /* Select FLL as a clock source for various peripherals */

  /* SIM_SOPT1: OSC32KSEL=0 */

  SIM_SOPT1 &= (uint32_t)~0x000C0000UL; /* System oscillator drives 32 kHz clock for various peripherals */

  /* Switch to FEI Mode */

  /* MCG_C1: CLKS=0,FRDIV=0,IREFS=1,IRCLKEN=1,IREFSTEN=0 */

  MCG_C1 = (uint8_t)0x06U;                            

  /* MCG_C2: LOCRE0=0,??=0,RANGE0=0,HGO0=0,EREFS0=0,LP=0,IRCS=0 */

  MCG_C2 = (uint8_t)0x00U;                            

  /* MCG_C4: DMX32=1,DRST_DRS=2 */

  MCG_C4 = (uint8_t)((MCG_C4 & (uint8_t)~(uint8_t)0x20U) | (uint8_t)0xC0U);

  /* OSC_CR: ERCLKEN=1,??=0,EREFSTEN=0,??=0,SC2P=0,SC4P=0,SC8P=0,SC16P=0 */

  OSC_CR = (uint8_t)0x80U;

  /* MCG_C7: OSCSEL=0 */

  MCG_C7 &= (uint8_t)~(uint8_t)0x01U;                          

  /* MCG_C5: ??=0,PLLCLKEN0=0,PLLSTEN0=0,PRDIV0=0 */

  MCG_C5 = (uint8_t)0x00U;                            

  /* MCG_C6: LOLIE0=0,PLLS=0,CME0=0,VDIV0=0 */

  MCG_C6 = (uint8_t)0x00U;                            

  while((MCG_S & MCG_S_IREFST_MASK) == 0x00U) { /* Check that the source of the FLL reference clock is the internal reference clock. */

  }

  while((MCG_S & 0x0CU) != 0x00U) {    /* Wait until output of the FLL is selected */

  }

  /*** End of PE initialization code after reset ***/

}

Cheers.

Labels (1)
Tags (3)
0 Kudos
Reply
4 Replies

2,721 Views
pavel_sadek
NXP Employee
NXP Employee

Hi

are you correctly trimming the internal clock?

if you are using PE tools (Multilink or OSJTAG), it looks as in the document

https://community.freescale.com/docs/DOC-95356

Pavel

0 Kudos
Reply

2,721 Views
Alex_HMBE
Contributor II

Thank you Pavel,

I am trimming the IRC to 32.768kHz. I went through to double check my setup and added the following two lines to copy the trim values into the registers:

  MCG_C3 = *((uint8_t*) 0x03FFU);

  MCG_C4 = (MCG_C4 & 0xE0U) | ((*((uint8_t*) 0x03FEU)) & 0x1FU);

This hasn't resolved the issue and the rest of my setup, as far as I can tell, is the same as what is shown in that document.

Regards,

Alex.

0 Kudos
Reply

2,721 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

I do a test based on TWR-K20D72M board, with using internal trim value 0x190 (MCG_C3 = 0X90; MCG_C4 [SCFTRIM] is set), I measure flexbus clock output frequency at PTC3 pin (ALT5 function is CLKOUT). I could measure the CLKOUT clock is not a stable 36MHz, which could swing from 36.4MHz to 36.0MHz. For the UART with clock error tolerance, the FLL with IRC(slow) could generate UART communication matched clock. I could get correct print characters from serial terminal with baud rate 115200.

Wish it helps.

0 Kudos
Reply

2,721 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I am checking with this issue, I will be back when I could get any updated info.

Thank you for the patience.

B.R.

Ma Hui

0 Kudos
Reply