We're trying to get the full 72MHz system clock out of a 64-pin, 72MHz K10. We've pulled code in from PE, setting the DCO up to give us 2197x32.768=71.99MHz. After setting up a UART and noticing some bad characters, I checked the bit period on a scope and found that it was off by 2.9% (after taking the baud rate error created by the UART divisor into account).
So, my question is - should the FLL output, using the IRC, be able to produce a reliable 72MHz?
Here's the setup code from PE:
void __init_hardware()
{
/*** PE initialization code after reset ***/
SCB_VTOR = (uint32_t)__vector_table; /* Set the interrupt vector table position */
/* Disable the WDOG module */
/* WDOG_UNLOCK: WDOGUNLOCK=0xC520 */
WDOG_UNLOCK = (uint16_t)0xC520U; /* Key 1 */
/* WDOG_UNLOCK : WDOGUNLOCK=0xD928 */
WDOG_UNLOCK = (uint16_t)0xD928U; /* Key 2 */
/* WDOG_STCTRLH: ??=0,DISTESTWDOG=0,BYTESEL=0,TESTSEL=0,TESTWDOG=0,??=0,??=1,WAITEN=1,STOPEN=1,DBGEN=0,ALLOWUPDATE=1,WINEN=0,IRQRSTEN=0,CLKSRC=1,WDOGEN=0 */
WDOG_STCTRLH = (uint16_t)0x01D2U;
/* System clock initialization */
/* SIM_SCGC5: PORTA=1 */
SIM_SCGC5 |= (uint32_t)0x0200UL; /* Enable clock gate for ports to enable pin routing */
/* SIM_CLKDIV1: OUTDIV1=0,OUTDIV2=1,OUTDIV3=3,OUTDIV4=3,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
SIM_CLKDIV1 = (uint32_t)0x01330000UL; /* Update system prescalers */
/* SIM_SOPT2: PLLFLLSEL=0 */
SIM_SOPT2 &= (uint32_t)~0x00010000UL; /* Select FLL as a clock source for various peripherals */
/* SIM_SOPT1: OSC32KSEL=0 */
SIM_SOPT1 &= (uint32_t)~0x000C0000UL; /* System oscillator drives 32 kHz clock for various peripherals */
/* Switch to FEI Mode */
/* MCG_C1: CLKS=0,FRDIV=0,IREFS=1,IRCLKEN=1,IREFSTEN=0 */
MCG_C1 = (uint8_t)0x06U;
/* MCG_C2: LOCRE0=0,??=0,RANGE0=0,HGO0=0,EREFS0=0,LP=0,IRCS=0 */
MCG_C2 = (uint8_t)0x00U;
/* MCG_C4: DMX32=1,DRST_DRS=2 */
MCG_C4 = (uint8_t)((MCG_C4 & (uint8_t)~(uint8_t)0x20U) | (uint8_t)0xC0U);
/* OSC_CR: ERCLKEN=1,??=0,EREFSTEN=0,??=0,SC2P=0,SC4P=0,SC8P=0,SC16P=0 */
OSC_CR = (uint8_t)0x80U;
/* MCG_C7: OSCSEL=0 */
MCG_C7 &= (uint8_t)~(uint8_t)0x01U;
/* MCG_C5: ??=0,PLLCLKEN0=0,PLLSTEN0=0,PRDIV0=0 */
MCG_C5 = (uint8_t)0x00U;
/* MCG_C6: LOLIE0=0,PLLS=0,CME0=0,VDIV0=0 */
MCG_C6 = (uint8_t)0x00U;
while((MCG_S & MCG_S_IREFST_MASK) == 0x00U) { /* Check that the source of the FLL reference clock is the internal reference clock. */
}
while((MCG_S & 0x0CU) != 0x00U) { /* Wait until output of the FLL is selected */
}
/*** End of PE initialization code after reset ***/
}
Cheers.
 
					
				
		
 pavel_sadek
		
			pavel_sadek
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi
are you correctly trimming the internal clock?
if you are using PE tools (Multilink or OSJTAG), it looks as in the document
https://community.freescale.com/docs/DOC-95356
Pavel
 
					
				
		
Thank you Pavel,
I am trimming the IRC to 32.768kHz. I went through to double check my setup and added the following two lines to copy the trim values into the registers:
MCG_C3 = *((uint8_t*) 0x03FFU);
MCG_C4 = (MCG_C4 & 0xE0U) | ((*((uint8_t*) 0x03FEU)) & 0x1FU);
This hasn't resolved the issue and the rest of my setup, as far as I can tell, is the same as what is shown in that document.
Regards,
Alex.
 
					
				
		
 Hui_Ma
		
			Hui_Ma
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I do a test based on TWR-K20D72M board, with using internal trim value 0x190 (MCG_C3 = 0X90; MCG_C4 [SCFTRIM] is set), I measure flexbus clock output frequency at PTC3 pin (ALT5 function is CLKOUT). I could measure the CLKOUT clock is not a stable 36MHz, which could swing from 36.4MHz to 36.0MHz. For the UART with clock error tolerance, the FLL with IRC(slow) could generate UART communication matched clock. I could get correct print characters from serial terminal with baud rate 115200.
Wish it helps.
 
					
				
		
 Hui_Ma
		
			Hui_Ma
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
I am checking with this issue, I will be back when I could get any updated info.
Thank you for the patience.
B.R.
Ma Hui