Connecting to image sensor with K series MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connecting to image sensor with K series MCU

ソリューションへジャンプ
1,701件の閲覧回数
josephchen
Contributor III

Is it possible to connect K63 to image sensor and retrieve pictures or video clips?

0 件の賞賛
返信
1 解決策
1,494件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

The demo is capturing the CMOS sensor using GPIO and sending the frames to display. It is a raw image and low resolution (QVGA) and low frame rate. No video player.

If you need to play video files, video streaming, compress/encode CMOS sensor stream, etc you need to go to more powerful device with the appropriated peripheral, look at the i.Mx family.

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,494件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Check this AN:

AN4627 
AN4627, Connecting Kinetis MCU with CMOS Sensor Interface through GPIO - Application Note

Luis

1,494件の閲覧回数
josephchen
Contributor III

Is it only for picture capturing or also including video clips?

Is the decompression necessary? By MCU or image sensor itself or external DSP?

0 件の賞賛
返信
1,495件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

The demo is capturing the CMOS sensor using GPIO and sending the frames to display. It is a raw image and low resolution (QVGA) and low frame rate. No video player.

If you need to play video files, video streaming, compress/encode CMOS sensor stream, etc you need to go to more powerful device with the appropriated peripheral, look at the i.Mx family.

Luis

0 件の賞賛
返信