This bit of code seems to kill my JTAG. None of these signals are associated with JTAG so I don't understand what the problem is. I have commented them out one after another and any one of the GPIO_PinInit functions kills the communication. The only one that kinda makes sense is PA4 being the EzPort CS/NMI but the rest of them make no sense at all. Any idea what I'm doing wrong here?
#define ANT_BOOT_PORT PORTA
#define ANT_BOOT_PIN 4
#define ANT_BOOT_CFG kGPIO_DigitalOutput
#define ANT_BOOT_MUX kPORT_MuxAsGpio
#define ANT_RST_PORT PORTA
#define ANT_RST_PIN 6
#define ANT_RST_CFG kGPIO_DigitalOutput
#define ANT_RST_MUX kPORT_MuxAsGpio
#define OLED_RS_PORT PORTA
#define OLED_RS_PIN 24
#define OLED_RS_CFG kGPIO_DigitalOutput
#define OLED_RS_MUX kPORT_MuxAsGpio
#define OLED_RST_PORT PORTA
#define OLED_RST_PIN 25
#define OLED_RST_CFG kGPIO_DigitalOutput
#define OLED_RST_MUX kPORT_MuxAsGpio
#define OLED_PWR_PORT PORTA
#define OLED_PWR_PIN 26
#define OLED_PWR_CFG kGPIO_DigitalOutput
#define OLED_PWR_MUX kPORT_MuxAsGpio
///////////////////////////////
////////// PORTA //////////////
///////////////////////////////
CLOCK_EnableClock(kCLOCK_PortA);
// GPIO
PORT_SetPinMux(ANT_BOOT_PORT, ANT_BOOT_PIN, ANT_BOOT_MUX);
PORT_SetPinMux(ANT_RST_PORT, ANT_RST_PIN, ANT_RST_MUX);
PORT_SetPinMux(OLED_RS_PORT, OLED_RS_PIN, OLED_RS_MUX);
PORT_SetPinMux(OLED_RST_PORT, OLED_RST_PIN, OLED_RST_MUX);
PORT_SetPinMux(OLED_PWR_PORT, OLED_PWR_PIN, OLED_PWR_MUX);
GPIO_PinInit(ANT_BOOT_PORT, ANT_BOOT_PIN, &(gpio_pin_config_t){ANT_BOOT_CFG, 0} ); // PA4
GPIO_PinInit(ANT_RST_PORT, ANT_RST_PIN, &(gpio_pin_config_t){ANT_RST_CFG, 0} ); // PA6
GPIO_PinInit(OLED_RS_PORT, OLED_RS_PIN, &(gpio_pin_config_t){OLED_RS_CFG, 0} ); // PA24
GPIO_PinInit(OLED_RST_PORT, OLED_RST_PIN, &(gpio_pin_config_t){OLED_RST_CFG, 0} ); // PA25
GPIO_PinInit(OLED_PWR_PORT, OLED_PWR_PIN, &(gpio_pin_config_t){OLED_PWR_CFG, 0} ); // PA26