This bit of code seems to kill my JTAG. None of these signals are associated with JTAG so I don't understand what the problem is. I have commented them out one after another and any one of the GPIO_PinInit functions kills the communication. The only one that kinda makes sense is PA4 being the EzPort CS/NMI but the rest of them make no sense at all. Any idea what I'm doing wrong here?
#define ANT_BOOT_PORT PORTA
#define ANT_BOOT_PIN 4
#define ANT_BOOT_CFG kGPIO_DigitalOutput
#define ANT_BOOT_MUX kPORT_MuxAsGpio
#define ANT_RST_PORT PORTA
#define ANT_RST_PIN 6
#define ANT_RST_CFG kGPIO_DigitalOutput
#define ANT_RST_MUX kPORT_MuxAsGpio
#define OLED_RS_PORT PORTA
#define OLED_RS_PIN 24
#define OLED_RS_CFG kGPIO_DigitalOutput
#define OLED_RS_MUX kPORT_MuxAsGpio
#define OLED_RST_PORT PORTA
#define OLED_RST_PIN 25
#define OLED_RST_CFG kGPIO_DigitalOutput
#define OLED_RST_MUX kPORT_MuxAsGpio
#define OLED_PWR_PORT PORTA
#define OLED_PWR_PIN 26
#define OLED_PWR_CFG kGPIO_DigitalOutput
#define OLED_PWR_MUX kPORT_MuxAsGpio
///////////////////////////////
////////// PORTA //////////////
///////////////////////////////
CLOCK_EnableClock(kCLOCK_PortA);
// GPIO
PORT_SetPinMux(ANT_BOOT_PORT, ANT_BOOT_PIN, ANT_BOOT_MUX);
PORT_SetPinMux(ANT_RST_PORT, ANT_RST_PIN, ANT_RST_MUX);
PORT_SetPinMux(OLED_RS_PORT, OLED_RS_PIN, OLED_RS_MUX);
PORT_SetPinMux(OLED_RST_PORT, OLED_RST_PIN, OLED_RST_MUX);
PORT_SetPinMux(OLED_PWR_PORT, OLED_PWR_PIN, OLED_PWR_MUX);
GPIO_PinInit(ANT_BOOT_PORT, ANT_BOOT_PIN, &(gpio_pin_config_t){ANT_BOOT_CFG, 0} ); // PA4
GPIO_PinInit(ANT_RST_PORT, ANT_RST_PIN, &(gpio_pin_config_t){ANT_RST_CFG, 0} ); // PA6
GPIO_PinInit(OLED_RS_PORT, OLED_RS_PIN, &(gpio_pin_config_t){OLED_RS_CFG, 0} ); // PA24
GPIO_PinInit(OLED_RST_PORT, OLED_RST_PIN, &(gpio_pin_config_t){OLED_RST_CFG, 0} ); // PA25
GPIO_PinInit(OLED_PWR_PORT, OLED_PWR_PIN, &(gpio_pin_config_t){OLED_PWR_CFG, 0} ); // PA26
已解决! 转到解答。
GPIO_PinInit should have been called with GPIOA rather than PORTA
#define ANT_BOOT_PORT PORTA
#define ANT_BOOT_GPIO GPIOA
#define ANT_BOOT_PIN 4
#define ANT_BOOT_CFG kGPIO_DigitalOutput
#define ANT_BOOT_MUX kPORT_MuxAsGpio
PORT_SetPinMux(ANT_BOOT_PORT, ANT_BOOT_PIN, ANT_BOOT_MUX);
GPIO_PinInit(ANT_BOOT_GPIO, ANT_BOOT_PIN, &(gpio_pin_config_t){ANT_BOOT_CFG, 0} ); // PA4
GPIO_PinInit should have been called with GPIOA rather than PORTA
#define ANT_BOOT_PORT PORTA
#define ANT_BOOT_GPIO GPIOA
#define ANT_BOOT_PIN 4
#define ANT_BOOT_CFG kGPIO_DigitalOutput
#define ANT_BOOT_MUX kPORT_MuxAsGpio
PORT_SetPinMux(ANT_BOOT_PORT, ANT_BOOT_PIN, ANT_BOOT_MUX);
GPIO_PinInit(ANT_BOOT_GPIO, ANT_BOOT_PIN, &(gpio_pin_config_t){ANT_BOOT_CFG, 0} ); // PA4
In fsl_gpio.h (standard KSDK code) you have
/*!
* @brief Sets the output level of the multiple GPIO pins to the logic 1 or 0.
*
* @param base GPIO peripheral base pointer (GPIOA, GPIOB, GPIOC, and so on.)
* @param pin GPIO pin number
* @param output GPIO pin output logic level.
* - 0: corresponding pin output low-logic level.
* - 1: corresponding pin output high-logic level.
*/
static inline void GPIO_PinWrite(GPIO_Type *base, uint32_t pin, uint8_t output)
{
if (output == 0U)
{
base->PCOR = 1U << pin;
}
else
{
base->PSOR = 1U << pin;
}
}
I'm pretty sure that should be
base->PCOR |= 1U << pin;
and
base->PSOR |= 1U << pin;