Configuring non-JTAG pins on PORTA breaks JTAG with K24

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring non-JTAG pins on PORTA breaks JTAG with K24

Jump to solution
1,549 Views
ryanlush
Contributor IV

This bit of code seems to kill my JTAG. None of these signals are associated with JTAG so I don't understand what the problem is. I have commented them out one after another and any one of the GPIO_PinInit functions kills the communication. The only one that kinda makes sense is PA4 being the EzPort CS/NMI but the rest of them make no sense at all. Any idea what I'm doing wrong here?

#define ANT_BOOT_PORT           PORTA
#define ANT_BOOT_PIN            4
#define ANT_BOOT_CFG            kGPIO_DigitalOutput
#define ANT_BOOT_MUX            kPORT_MuxAsGpio
        
#define ANT_RST_PORT            PORTA
#define ANT_RST_PIN             6
#define ANT_RST_CFG             kGPIO_DigitalOutput
#define ANT_RST_MUX             kPORT_MuxAsGpio
        
#define OLED_RS_PORT            PORTA
#define OLED_RS_PIN             24
#define OLED_RS_CFG             kGPIO_DigitalOutput
#define OLED_RS_MUX             kPORT_MuxAsGpio
        
#define OLED_RST_PORT           PORTA
#define OLED_RST_PIN            25
#define OLED_RST_CFG            kGPIO_DigitalOutput
#define OLED_RST_MUX            kPORT_MuxAsGpio
        
#define OLED_PWR_PORT           PORTA
#define OLED_PWR_PIN            26
#define OLED_PWR_CFG            kGPIO_DigitalOutput
#define OLED_PWR_MUX            kPORT_MuxAsGpio

    ///////////////////////////////
    ////////// PORTA //////////////
    ///////////////////////////////
    CLOCK_EnableClock(kCLOCK_PortA);

    // GPIO    
    PORT_SetPinMux(ANT_BOOT_PORT,  ANT_BOOT_PIN, ANT_BOOT_MUX);         
    PORT_SetPinMux(ANT_RST_PORT,   ANT_RST_PIN,  ANT_RST_MUX);         
    PORT_SetPinMux(OLED_RS_PORT,   OLED_RS_PIN,  OLED_RS_MUX);         
    PORT_SetPinMux(OLED_RST_PORT,  OLED_RST_PIN, OLED_RST_MUX);         
    PORT_SetPinMux(OLED_PWR_PORT,  OLED_PWR_PIN, OLED_PWR_MUX);         

    GPIO_PinInit(ANT_BOOT_PORT,  ANT_BOOT_PIN, &(gpio_pin_config_t){ANT_BOOT_CFG, 0} );      // PA4
    GPIO_PinInit(ANT_RST_PORT,   ANT_RST_PIN,  &(gpio_pin_config_t){ANT_RST_CFG,  0} );            // PA6
    GPIO_PinInit(OLED_RS_PORT,   OLED_RS_PIN,  &(gpio_pin_config_t){OLED_RS_CFG,  0} );           // PA24
    GPIO_PinInit(OLED_RST_PORT,  OLED_RST_PIN, &(gpio_pin_config_t){OLED_RST_CFG, 0} );        // PA25
    GPIO_PinInit(OLED_PWR_PORT,  OLED_PWR_PIN, &(gpio_pin_config_t){OLED_PWR_CFG, 0} );    // PA26

Labels (1)
0 Kudos
Reply
1 Solution
1,394 Views
ryanlush
Contributor IV

GPIO_PinInit should have been called with GPIOA rather than PORTA

#define ANT_BOOT_PORT           PORTA

#define ANT_BOOT_GPIO           GPIOA
#define ANT_BOOT_PIN             4
#define ANT_BOOT_CFG            kGPIO_DigitalOutput
#define ANT_BOOT_MUX            kPORT_MuxAsGpio

PORT_SetPinMux(ANT_BOOT_PORT,  ANT_BOOT_PIN, ANT_BOOT_MUX);  

GPIO_PinInit(ANT_BOOT_GPIO,  ANT_BOOT_PIN, &(gpio_pin_config_t){ANT_BOOT_CFG, 0} );      // PA4

View solution in original post

0 Kudos
Reply
3 Replies
1,395 Views
ryanlush
Contributor IV

GPIO_PinInit should have been called with GPIOA rather than PORTA

#define ANT_BOOT_PORT           PORTA

#define ANT_BOOT_GPIO           GPIOA
#define ANT_BOOT_PIN             4
#define ANT_BOOT_CFG            kGPIO_DigitalOutput
#define ANT_BOOT_MUX            kPORT_MuxAsGpio

PORT_SetPinMux(ANT_BOOT_PORT,  ANT_BOOT_PIN, ANT_BOOT_MUX);  

GPIO_PinInit(ANT_BOOT_GPIO,  ANT_BOOT_PIN, &(gpio_pin_config_t){ANT_BOOT_CFG, 0} );      // PA4

0 Kudos
Reply
1,394 Views
ryanlush
Contributor IV

In fsl_gpio.h (standard KSDK code) you have

/*!
 * @brief Sets the output level of the multiple GPIO pins to the logic 1 or 0.
 *
 * @param base    GPIO peripheral base pointer (GPIOA, GPIOB, GPIOC, and so on.)
 * @param pin     GPIO pin number
 * @param output  GPIO pin output logic level.
 *        - 0: corresponding pin output low-logic level.
 *        - 1: corresponding pin output high-logic level.
 */
static inline void GPIO_PinWrite(GPIO_Type *base, uint32_t pin, uint8_t output)
{
    if (output == 0U)
    {
        base->PCOR = 1U << pin;
    }
    else
    {
        base->PSOR = 1U << pin;
    }
}

I'm pretty sure that should be

base->PCOR |= 1U << pin;

and

base->PSOR |= 1U << pin;

0 Kudos
Reply
1,394 Views
ryanlush
Contributor IV

I'm wrong. Writing a 0 to those registers has no effect. Still lost...

0 Kudos
Reply