CodeWarrior support for MK60X256VLQ100

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior support for MK60X256VLQ100

跳至解决方案
1,210 次查看
WadeJones
Contributor I

I'm working on my first project using CodeWarrior and I have a question regarding support for the Kinetis MK60X256VLQ100, which is the LQFP144 package. When I create the project and select the MK60 family, I only see support for the BGA package when I try to use the Device Initialization tool. I know I must be missing a selection somewhere, but I can't see it. Thanks for any help anyone might be able to provide.

标签 (1)
0 项奖励
回复
1 解答
1,102 次查看
apanecatl
Senior Contributor II

Once you create the project selecting the processor variant (MK60DX256 / MK60DX256Z) and the Device Initialization tool, go to the Target CPU tab, and click on Select CPU package, a small window will pop up showing you the available packages, select MK60DX256VLQ10 (144 LQFP) and you're right on track.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,103 次查看
apanecatl
Senior Contributor II

Once you create the project selecting the processor variant (MK60DX256 / MK60DX256Z) and the Device Initialization tool, go to the Target CPU tab, and click on Select CPU package, a small window will pop up showing you the available packages, select MK60DX256VLQ10 (144 LQFP) and you're right on track.

0 项奖励
回复
1,102 次查看
WadeJones
Contributor I

That worked. Thanks for the help.

0 项奖励
回复