'Clear endpoint halt failed' FRDM-KL25Z HID during compliance tool test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

'Clear endpoint halt failed' FRDM-KL25Z HID during compliance tool test

1,299 Views
bobpaddock
Senior Contributor III

I'm trying to bring up a Generic HID (this is not a keyboard or mouse) on the Freedom Board FRDM-KL25Z, Kinetis MKL25Z128.

Has anyone else used, or run into problems with the USB Consortium's Command Verifier Tool, USB20CV R1.4.9.7,  against Kinetis parts?

http://www.usb.org/developers/tools/

When I run the USB 2. 0 Command Verifier tool on Windows7x64 I always get:

"ERROR   Clear endpoint halt failed".  Other tests always pass.

I'm hoping someone here can shed some light on why this test is failing the compliance check.

I've included a bus capture and the setup_endpoint() code below.

These Halt tests take ten seconds to run, while all the other tests take one second to run.

This seems suspicious to me.  Is it normal for this Halt Feature test to take so long?

Below is three test runs of the Halt Endpoint Test, in Command Verifier.

First run is code returning the current status of the Halt bit, as the code should work.

Second run status always returns zero, and the third run status always returns 0x0001, to prove that changing the code changes the test results.

Halt Endpoint Test : Failed

INFO    Start time: Wed Jul 31 09:55:25 2013

INFO    Testing Interface number : 0 Alternate setting : 0

INFO    Testing EndPoint type : Interrupt, Address : 81

INFO    Endpoint is currently not halted

INFO    Endpoint is halted

ERROR   Clear endpoint halt failed

INFO    Cleared endpoint halt

FAIL    (1.2.91) A device that has Bulk/Interrupt endpoints must support the

        Halt Endpoint request on those endpoints.

INFO    Testing EndPoint type : Interrupt, Address : 2

INFO    Endpoint is currently not halted

INFO    Endpoint is halted

ERROR   Clear endpoint halt failed

INFO    Cleared endpoint halt

FAIL    (1.2.91) A device that has Bulk/Interrupt endpoints must support the

        Halt Endpoint request on those endpoints.

INFO    Stop time: Wed Jul 31 09:55:36 2013

INFO    Duration:  11 seconds.  {This is a lot longer than an of the other tests take.}

INFO    Stopping Test [ Halt Endpoint Test (Configuration Index 0):

     Number of: Fails (2); Aborts (0); Warnings (0) ]

This test is run with mGET_STATUS returning zero on all requests:

INFO    Start time: Wed Jul 31 10:02:30 2013

INFO    Testing Interface number : 0 Alternate setting : 0

INFO    Testing EndPoint type : Interrupt, Address : 81

INFO    Endpoint is currently not halted

ERROR   Endpoint could not be halted

ERROR   Clear endpoint halt failed

INFO    Cleared endpoint halt

FAIL    (1.2.91) A device that has Bulk/Interrupt endpoints must support the

        Halt Endpoint request on those endpoints.

INFO    Testing EndPoint type : Interrupt, Address : 2

INFO    Endpoint is currently not halted

ERROR   Endpoint could not be halted

ERROR   Clear endpoint halt failed

INFO    Cleared endpoint halt

FAIL    (1.2.91) A device that has Bulk/Interrupt endpoints must support the

        Halt Endpoint request on those endpoints.

INFO    Stop time: Wed Jul 31 10:02:41 2013

INFO    Duration:  11 seconds.  {This is a lot longer than an of the other tests take.}

INFO    Stopping Test [ Halt Endpoint Test (Configuration Index 0):

     Number of: Fails (2); Aborts (0); Warnings (0) ]

Test run with status always returning 0x0001:

Halt Endpoint Test : Failed

INFO    Start time: Wed Jul 31 10:14:29 2013

INFO    Testing Interface number : 0 Alternate setting : 0

INFO    Testing EndPoint type : Interrupt, Address : 81

INFO    Endpoint is currently halted

ERROR   Clear endpoint halt failed

ERROR   Could not clear endpoint halt

INFO    Endpoint is halted

ERROR   Clear endpoint halt failed

ERROR   Could not clear endpoint halt

FAIL    (1.2.91) A device that has Bulk/Interrupt endpoints must support the

        Halt Endpoint request on those endpoints.

INFO    Testing EndPoint type : Interrupt, Address : 2

INFO    Endpoint is currently halted

ERROR   Clear endpoint halt failed

ERROR   Could not clear endpoint halt

INFO    Endpoint is halted

ERROR   Clear endpoint halt failed

ERROR   Could not clear endpoint halt

FAIL    (1.2.91) A device that has Bulk/Interrupt endpoints must support the

        Halt Endpoint request on those endpoints.

INFO    Stop time: Wed Jul 31 10:14:50 2013

INFO    Duration:  21 seconds. {Even longer time.}

INFO    Stopping Test [ Halt Endpoint Test (Configuration Index 0):

     Number of: Fails (2); Aborts (0); Warnings (0) ]

Bus capture:

[Removed previous enumeration messages to keep this a reasonable length.]

2.087820167,GET_INTERFACE

2.087820167,DATA0,81,0A,00,00,00,00,01,00,DD,C8,

2.087828792,ACK

2.087837083,IN Add:2 EndPoint:0

2.087840375,NAK

2.087849083,IN Add:2 EndPoint:0

2.087852375,DATA1,00,40,BF,

2.087856750,ACK

2.087862917,OUT Add:2 EndPoint:0

2.087866167,DATA1,00,00,

2.087869458,ACK

2.089087625,SETUP Add:2 EndPoint:0

2.089090875,GET_STATUS

2.089090875,DATA0,82,00,00,00,81,00,02,00,1F,11,

2.089099500,ACK

2.089108875,IN Add:2 EndPoint:0

2.089112167,DATA1,00,00,FE,4F,

2.089117208,ACK

2.089130125,OUT Add:2 EndPoint:0

2.089133375,DATA1,00,00,

2.089136667,ACK

2.090311167,SETUP Add:2 EndPoint:0

2.090314417,SET_FEATURE

2.090314417,DATA0,02,03,00,00,81,00,00,00,25,11,

2.090323042,ACK

2.090331333,IN Add:2 EndPoint:0

2.090334625,DATA1,00,00,

2.090338250,ACK

2.090811167,SETUP Add:2 EndPoint:0

2.090814417,GET_STATUS

2.090814417,DATA0,82,00,00,00,81,00,02,00,1F,11,

2.090823042,ACK

2.090831750,IN Add:2 EndPoint:0

2.090835042,DATA1,01,00,FF,DF,

2.090840083,ACK

2.090849000,OUT Add:2 EndPoint:0

2.090852250,DATA1,00,00,

2.090855542,ACK

2.092060875,SETUP Add:2 EndPoint:0

2.092064125,CLEAR_FEATURE

2.092064125,DATA0,02,01,00,00,81,00,00,00,06,D1,

2.092072750,ACK

2.092081792,IN Add:2 EndPoint:0

2.092085083,DATA0,00,00,

2.092088708,ACK

[Long gap of only Start of Frames here. Why?]

7.095046917,SETUP Add:2 EndPoint:0

7.095050167,GET_STATUS

7.095050167,DATA0,82,00,00,00,81,00,02,00,1F,11,

7.095058792,ACK

7.095067167,IN Add:2 EndPoint:0

7.095070458,DATA1,00,00,FE,4F,

7.095075417,ACK

7.095081000,OUT Add:2 EndPoint:0

7.095084250,DATA1,00,00,

7.095087542,ACK

7.097046667,SETUP Add:2 EndPoint:0

7.097049917,GET_STATUS

7.097049917,DATA0,82,00,00,00,02,00,02,00,36,95,

7.097058542,ACK

7.097066917,IN Add:2 EndPoint:0

7.097070208,DATA1,00,00,FE,4F,

7.097075167,ACK

7.097080750,OUT Add:2 EndPoint:0

7.097084000,DATA1,00,00,

7.097087292,ACK

7.098296708,SETUP Add:2 EndPoint:0

7.098299958,SET_FEATURE

7.098299958,DATA0,02,03,00,00,02,00,00,00,0C,95,

7.098308583,ACK

7.098317292,IN Add:2 EndPoint:0

7.098320583,DATA1,00,00,

7.098324208,ACK

7.099546167,SETUP Add:2 EndPoint:0

7.099549417,GET_STATUS

7.099549417,DATA0,82,00,00,00,02,00,02,00,36,95,

7.099558042,ACK

7.099566917,IN Add:2 EndPoint:0

7.099570208,DATA1,01,00,FF,DF,

7.099575333,ACK

7.099584083,OUT Add:2 EndPoint:0

7.099587333,DATA1,00,00,

7.099590625,ACK

7.100800375,SETUP Add:2 EndPoint:0

7.100803625,CLEAR_FEATURE

7.100803625,DATA0,02,01,00,00,02,00,00,00,2F,55,

7.100812250,ACK

7.100820875,IN Add:2 EndPoint:0

7.100824167,DATA0,00,00,

7.100827792,ACK

[Long gap of only Start of Frames here. Why?]

12.104906625,SETUP Add:2 EndPoint:0

12.104909875,GET_STATUS

12.104909875,DATA0,82,00,00,00,02,00,02,00,36,95,

12.104918500,ACK

12.104926958,IN Add:2 EndPoint:0

12.104930250,DATA1,00,00,FE,4F,

12.104935291,ACK

12.104944041,OUT Add:2 EndPoint:0

12.104947291,DATA1,00,00,

12.104950583,ACK

[Nothing but Start of Frames from here on.]

Endpoint feature source:

static void usb_setup_endpoint( endpoint_t *const ep_ptr, USB_SETUP *const setup_ptr )

{

  uint16_t status_u16 = 0U;

  uint_fast8_t const ep_u8 = (setup_ptr->wIndex & 0x0FU);

  switch( setup_ptr->bRequest )

    {

    case mCLR_FEATURE:

      ep_ptr->features_u8 &= (uint8_t) ~FEATURE_ENDPOINT_HALT_MASK;

      /* Clear_Feature(ENDPOINT_HALT) resets the ednpoint's data toggle to DATA0: */

      ep_ptr->data01_u8 = BD_DATA0_MASK;

      // USB0_ENDPT( ep_u8 ) &= ~USB_ENDPT_EPSTALL_MASK; /* Commented out for testing to see if problem is hardware or returned status */

      usb_tx( ep_ptr, 0U, NULL ); /* ACK */

      break;

    case mSET_FEATURE:

      ep_ptr->features_u8 |= (uint8_t) FEATURE_ENDPOINT_HALT_MASK;

      //  USB0_ENDPT( ep_u8 ) |= USB_ENDPT_EPSTALL_MASK; /* Commented out for testing to see if problem is hardware or returned status */

      usb_tx( ep_ptr, 0U, NULL ); /* ACK */

      break;

    case mGET_STATUS:

      if( 0 != (FEATURE_ENDPOINT_HALT_MASK & ep_ptr->features_u8) )

        {

          status_u16 = FEATURE_ENDPOINT_HALT_MASK;

        }

      //      status_u16 = 0x0000U; // TESTING run two

      //      status_u16 = 0x0001U; // TESTING run three

      usb_queue_tx( ep_ptr, 2U, (uint8_t *const) &status_u16 ); /* Processor is Little Endian */

      break;

    default:

      iprintf("%u:EP[%u] ? R:0x%02X V:%u I:%u St:%u\r\n", __LINE__, ep_u8, setup_ptr->bRequest, setup_ptr->wValue, setup_ptr->wIndex, device_state_u8 );

      ep_stall( ep_u8 );

      break;

    }

}

Clear_Feature(ENDPOINT_HALT) is being done in SetConfig and SetInterface per the USB 2.0 spec.

Doesn't matter if the USB0_ENDPT() is commented out or not, results are the same.

Any insights?

0 Kudos
Reply
0 Replies