Change Project MCU from MKE06Z128VLD4 to MKE06Z64VLD4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change Project MCU from MKE06Z128VLD4 to MKE06Z64VLD4

469 Views
stevenlutz
Contributor II

I have a project working on the FRDM-MKE06Z. I then programmed my prototype board which was using a MKE06Z128VLD4 and worked just fine. 

I then realized that my project was using less than half of the 128k, so I tried installing a MKE06Z64VLD4 on the same prototype board, and it doesn't work. 

I then tried installing the MKE06Z64VLD4 , programming the chip is successful but the board no longer works. 
I then Downloaded and installed the MKE06Z specific SDK, an switching the MCU in MCUXpresso, but the project no longer compiles. 

Where am I going wrong in moving my project to the 64K from the 128k version of the chip?


Labels (1)
0 Kudos
1 Reply

391 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hello, Steven

After downloading the specific SDK for the replacement

MCU (MKE06Z64xxx4). I recommend you to create a new project selecting the KE06. Then make

sure that MKE06Z64xxx4 is highlighted. And finally, import your application files.

Capture.PNG 

Please let me know if this is useful.

 
Have a great day,
Diego

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos