Cavalier treatment of status returns in 5.0 Usb_Composite_Requests() in usb_composite.c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cavalier treatment of status returns in 5.0 Usb_Composite_Requests() in usb_composite.c

558 Views
johnstrohm
Contributor III

In the Freescale 5.0 Beta USB stack, in file usb_composite.c, in routine Usb_Composite_Requests(), the following lines appear (line numbers added for convenience):

456:                    USB_HID_Requests(setup_packet,data,size,(void *)devicePtr->hid_handle);

468:                USB_Audio_Requests(setup_packet,data,size,(void *)devicePtr->audio_handle);

478:                        status = USB_CDC_Other_Requests(setup_packet,data,size, (void *)devicePtr->cdc_handle);

490:                        status = USB_MSC_Requests(setup_packet,data,size, (void *)devicePtr->msc_handle);

504:                    USB_PHDC_Requests(setup_packet,data,size,(void *)devicePtr->phdc_handle);

USB_HID_Requests() returns a status.

USB_Audio_Requests() returns a status.  (Also, usb_audio.c contains a prototype for Usb_Audio_Other_Requests().  That should probably change to Usb_Audio_Requests().)

USB_PHDC_Requests() returns a status.

All of them may return error status, not just USB_OK.

The lines should probably be changed to:

456:                    status = USB_HID_Requests(setup_packet,data,size,(void *)devicePtr->hid_handle);

468:                status = USB_Audio_Requests(setup_packet,data,size,(void *)devicePtr->audio_handle);

478:                        status = USB_CDC_Other_Requests(setup_packet,data,size, (void *)devicePtr->cdc_handle);

490:                        status = USB_MSC_Requests(setup_packet,data,size, (void *)devicePtr->msc_handle);

504:                    status = USB_PHDC_Requests(setup_packet,data,size,(void *)devicePtr->phdc_handle);

Labels (2)
Tags (2)
0 Kudos
1 Reply

401 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi John,

Thanks for the report! I have forwarded your suggestion to our USB stack team and they will fix it in the future. I will update when I have any more information.

Thanks again and Best Regards,

Kan

0 Kudos