Hi denisc7slzo,
Please put the attached bin file into the FRDM-KL46Z driver. Does the D5 LED blink red?
If so, please try to debug your project with MCUXpresso IDE v11.6.1_8255.
If D5 LED doesn't blink red. Then you may need to use the Kinetis_Recovery_Utility discussed in "MK60DX256VLL10" RESET PIN
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------