Cannot connect to FRDM-KE04Z, frustrated!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot connect to FRDM-KE04Z, frustrated!

1,699 次查看
mikesilva
Contributor II

I've just spent a terrible, awful, horrible week trying to connect my toolset to a FRDM-KE04Z.  Details:

1) My development platform is an iMac, which also runs Windows 10 via Parallels.

2) Toolset is Rowley Crossworks, which I've used for years with other controller families.  For the KE04Z board it offers connections via Segger J-Link, P&EMicro, and CMSIS-DAP (among many others).

3) I can run Crossworks under OS-X or Windows.  I'd prefer OS-X, but I'll run under Windows if I have to.

4) I have no problem in either OS seeing the KE04Z board in Bootloader mode

5) I can drag-download any of the 3 OpenSDA apps found in the Quick Start package with apparent success.

6) I can also drag-download the Segger OpenSDA file with apparent success.

7) I believe I have installed any required drivers.

But under no circumstances have I been able to connect to the target board using any of the 3 protocols.  Using either OS.  After an entire week of fussing around!

I sense that there is something vague in the instructions that I am not understanding.  I really need some help.  The alternative is abandoning the Kinetis family altogether.

Thanks,

Mike

0 项奖励
回复
4 回复数

1,412 次查看
mikesilva
Contributor II

What comes from the NXP FRDM-KE04Z page for CMSIS-DAP is "CMSIS-DAP_OpenSDA.S19"  Not a .SDA file, which is mysterious but OK.  I tried plunking the file onto the board after putting the board into BOOTLOADER mode, but nothing happened - at least, nothing good.  Can you tell me how you would expect this to work (each step) if starting with a pristine FRDM-KE04Z board?  Thanks again.

Mike

0 项奖励
回复

1,412 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Mike,

The application note illustrates the way to implement the OpenSDA interface, so I'd highly recommend you to refer to it for details.

OpenSDA on the Freedom KL25Z Board | MCU on Eclipse
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,412 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

You can have a look to:

openSDA for Mac OS X

OpenOCD, Mac OS, FRDM-K64F
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,412 次查看
mjbcswitzerland
Specialist V

Mike

For Crossworks you need to use the DMSIS-DAP debugger.

If you have problems with it, it is best to contact Rowley since they may be able to help best.

You could also install IAR KickStart since this is adequate for the KE04 - it works fine with DEBUG-APP_Pemicro_v107.SDA. Also NXP's KDS will do it.

Regards

Mark

0 项奖励
回复