Can we use high-speed on FRDM K64 with additionnal chips

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use high-speed on FRDM K64 with additionnal chips

Jump to solution
1,486 Views
flauberttagu
Contributor III

Hello,

I want to know if the FRDM K64 which is using only full-speed USB could work with high-speed chips like the Texas instrument TUSB216RWBT.
If yes, will it be possible to increase the speed.

Thank you for your help in advance.

Regards.

Labels (2)
0 Kudos
1 Solution
1,392 Views
mjbcswitzerland
Specialist V

Hi

The K64 can only be used for low or full-speed USB device/host/OTG. To use it at high speed an external HS USB controller would be needed (eg. via SPI).
If your design needs HS USB operation it is simpler to move to the K65/K66 instead, which then allows one low/full speed OTG interface plus one low/full/high speed one.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]

View solution in original post

0 Kudos
4 Replies
1,392 Views
nxf56274
NXP Employee
NXP Employee

Hi,

1 Yes.

pastedImage_2.png

2 No. Full-speed and low speed. 

pastedImage_1.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,392 Views
flauberttagu
Contributor III

Dear Da Li,

Thank you for your quick answer.

Excellent day !

0 Kudos
1,393 Views
mjbcswitzerland
Specialist V

Hi

The K64 can only be used for low or full-speed USB device/host/OTG. To use it at high speed an external HS USB controller would be needed (eg. via SPI).
If your design needs HS USB operation it is simpler to move to the K65/K66 instead, which then allows one low/full speed OTG interface plus one low/full/high speed one.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]

0 Kudos
1,352 Views
flauberttagu
Contributor III

Hello,

Is it possible to move easily from a code develop for the K64 to the K65 or K66? Are those two ARM compatible to K64 in terms of computing?

Thx is andvance.

0 Kudos