Can we use high-speed on FRDM K64 with additionnal chips

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can we use high-speed on FRDM K64 with additionnal chips

跳至解决方案
2,818 次查看
flauberttagu
Contributor III

Hello,

I want to know if the FRDM K64 which is using only full-speed USB could work with high-speed chips like the Texas instrument TUSB216RWBT.
If yes, will it be possible to increase the speed.

Thank you for your help in advance.

Regards.

标签 (2)
0 项奖励
回复
1 解答
2,724 次查看
mjbcswitzerland
Specialist V

Hi

The K64 can only be used for low or full-speed USB device/host/OTG. To use it at high speed an external HS USB controller would be needed (eg. via SPI).
If your design needs HS USB operation it is simpler to move to the K65/K66 instead, which then allows one low/full speed OTG interface plus one low/full/high speed one.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,724 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

1 Yes.

pastedImage_2.png

2 No. Full-speed and low speed. 

pastedImage_1.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,724 次查看
flauberttagu
Contributor III

Dear Da Li,

Thank you for your quick answer.

Excellent day !

0 项奖励
回复
2,725 次查看
mjbcswitzerland
Specialist V

Hi

The K64 can only be used for low or full-speed USB device/host/OTG. To use it at high speed an external HS USB controller would be needed (eg. via SPI).
If your design needs HS USB operation it is simpler to move to the K65/K66 instead, which then allows one low/full speed OTG interface plus one low/full/high speed one.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]

0 项奖励
回复
2,684 次查看
flauberttagu
Contributor III

Hello,

Is it possible to move easily from a code develop for the K64 to the K65 or K66? Are those two ARM compatible to K64 in terms of computing?

Thx is andvance.

0 项奖励
回复