Can we use a pin other than Port A18 to pick up the 50MHz clock in..?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use a pin other than Port A18 to pick up the 50MHz clock in..?

677 Views
MWMinor
Contributor V

We have a custom K60DN512-based board which uses a 50MHz external clock input to the processor on PTA18 just like the TWR-K60D100M board. Unfortunately one of the printed circuit boards has lost the pad at M12, so we can't use the PTA18 input. Is it possible to re-programme the device to look for the clock on a different I/O pin or port...?

We are using Codewarrior V10.6 and running MQX4.1.

Thanks

Ken

Labels (1)
0 Kudos
Reply
1 Reply

546 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Ken Armitage

According to the reference manual, no, Unfortunately there isn't another pin that can be used as External clock/Oscillator input. Sorry for this inconvenience.


Hope this could help
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply