Can't make the watchdog timer interrupt to work in Freescale K60 microcontroller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't make the watchdog timer interrupt to work in Freescale K60 microcontroller

3,523 次查看
yoffie
Contributor I
Hi, Did anyone have any problems with making the WDOG interrupt working? Did anyone make it to work? Everything looks okay in my code, however WDOG interrupt is not generated before WDOG reset. (WDOG interrupt is enabled is NVIC, IRQRSTEN bit is set in WDOG ctrl register) Other than that, all other WDOG features work properly. Thanks, Yoffie
0 项奖励
回复
4 回复数

1,951 次查看
konrada
Contributor IV

I get WDOG interrupts on the K70, but...

  1. if the handler is in external RAM, most of the 256 cycles will be wasted waiting for instructions to be fetched
  2. breakpoints in the handler aren't reached.

How do you check whether your ISR is run? You could write a magic constant into a VBAT register (which survives reset).

0 项奖励
回复

1,951 次查看
Nana
Contributor II

I have the same problem, do you find any solution to this problem ?

All my wdog futures seems to work ok only the interrupt don't work ! I'm not using the MQX RTOS!

0 项奖励
回复

1,951 次查看
ignisuti
Contributor IV

Also having a issue with this. Here is what I have. Can someone from support please respond to this thread?

 

void WATCHDOG__initialize  (  void  )    {    /* Enable interrupts for Watchdog. */    ARM_CORTEX_M4__enable_interrupt( INT_Watchdog );             /* Unlock and enable the Watchdog timer. Configure interrupt. */    WDOG_UNLOCK = 0xC520;  WDOG_UNLOCK = 0xD928;    WDOG_STCTRLH |= WDOG_STCTRLH_WDOGEN_MASK;    WDOG_STCTRLH |= WDOG_STCTRLH_IRQRSTEN_MASK;        } /* WATCHDOG__initialize() */

 

0 项奖励
回复

1,951 次查看
ignisuti
Contributor IV

Update on my earlier post...

I thought my code would set the IRQRSTEN bit, but when I stepped through the debug code, I could see it was not. This is because that register only allows writing to it once during a change period.

 

So, by combining two lines into one, I was able to get my interrupts working. 

 

WDOG_STCTRLH |= WDOG_STCTRLH_WDOGEN_MASK | WDOG_STCTRLH_IRQRSTEN_MASK;

 


0 项奖励
回复