Can't connect to TWR-KV31f120M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't connect to TWR-KV31f120M

Jump to solution
1,685 Views
GaryOlmstead
Senior Contributor I

I have two TWR-KV31F120M boards.  When I connect a USB cable to either board, the power LED comes on, but I don't get a "USB Drive Detected" pop-up window, and Windows 10 Device Manager never shows a Ports(COM and LPT) entry. MCUxpresso 11.5.0 can't make contact. Hitting Reset doesn't help.  It doesn't matter if the Tower elevator modules are in place or not.

With the same cable plugged into a FRDM-KV31, I get the pop-up and Device Manager Ports entry, and MCUxpresso contact, so I know that the computer and cable are OK.

Any suggestions?

 

0 Kudos
Reply
1 Solution
1,674 Views
GaryOlmstead
Senior Contributor I

Never mind, I figured it out (had to reload the bootloader).  Both boards work now.

View solution in original post

0 Kudos
Reply
2 Replies
1,675 Views
GaryOlmstead
Senior Contributor I

Never mind, I figured it out (had to reload the bootloader).  Both boards work now.

0 Kudos
Reply
1,684 Views
GaryOlmstead
Senior Contributor I

Forgot mention that I have double-checked that ALL jumpers are in the default position on both boards.

0 Kudos
Reply