Can't connect to TWR-KV31f120M

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't connect to TWR-KV31f120M

跳至解决方案
1,627 次查看
GaryOlmstead
Senior Contributor I

I have two TWR-KV31F120M boards.  When I connect a USB cable to either board, the power LED comes on, but I don't get a "USB Drive Detected" pop-up window, and Windows 10 Device Manager never shows a Ports(COM and LPT) entry. MCUxpresso 11.5.0 can't make contact. Hitting Reset doesn't help.  It doesn't matter if the Tower elevator modules are in place or not.

With the same cable plugged into a FRDM-KV31, I get the pop-up and Device Manager Ports entry, and MCUxpresso contact, so I know that the computer and cable are OK.

Any suggestions?

 

0 项奖励
回复
1 解答
1,616 次查看
GaryOlmstead
Senior Contributor I

Never mind, I figured it out (had to reload the bootloader).  Both boards work now.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,617 次查看
GaryOlmstead
Senior Contributor I

Never mind, I figured it out (had to reload the bootloader).  Both boards work now.

0 项奖励
回复
1,626 次查看
GaryOlmstead
Senior Contributor I

Forgot mention that I have double-checked that ALL jumpers are in the default position on both boards.

0 项奖励
回复