Can period measurement be performed on a ramp signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can period measurement be performed on a ramp signal

848 Views
sivatelasula
Contributor I

Hello,

I am using K10 processor to perform period measurement on a ramp signal as shown here:

Capture.PNG

Is this possible using the "Dual Edge Capture mode" with rising edge as the edge to be monitored? Or is the measurement limited to rectangular type signals.

If this is possible, and I use Channel 0 on FTM0 as the input for the signal, then should I explicitly set anything on Ch1 of FTM0. I am using Processor Expert to configure the peripheral.

with regards,

Siva Telasula

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

677 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Siva

If the signal is quite neat, I think it's OK. Or, if there is some noise around the critical point, the result is not guaranteed. Yes, you need to set clearly on FTM channel.I think you also can consider CMP for your period measurement. CMP support hysteresis feature, if signal are with noise, it's a better way.

Hope my reply can help you.

Best Regards

Paul

0 Kudos
Reply