Can a Kinetis K70 be soft reset but still maintain the contents of external DDR2 accessed through the DDRMC for use after the restart?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can a Kinetis K70 be soft reset but still maintain the contents of external DDR2 accessed through the DDRMC for use after the restart?

Jump to solution
1,109 Views
evalproj
Contributor I

Can a Kinetis K70 be soft reset but still maintain the contents of external DDR2 accessed through the DDRMC for use after the restart?

Labels (1)
0 Kudos
Reply
1 Solution
883 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi xx ofeval,

    As you know, if the power is not off, the contents of the external DDR2 will be still stored.

  The soft reset won't power off the DDR2, so the contests in DDR2 won't be lost.

  But, about the access through the DDRMC, you can check the DDR register, you will find, if the MCU is reset, no matter soft or hardware reset, the DDR register will back to the reset data, so you need to configure the DDR register again after the software reset, then the external DDR2 can be accessed again.

Wish it helps you!

If you still have question, please contact with me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
884 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi xx ofeval,

    As you know, if the power is not off, the contents of the external DDR2 will be still stored.

  The soft reset won't power off the DDR2, so the contests in DDR2 won't be lost.

  But, about the access through the DDRMC, you can check the DDR register, you will find, if the MCU is reset, no matter soft or hardware reset, the DDR register will back to the reset data, so you need to configure the DDR register again after the software reset, then the external DDR2 can be accessed again.

Wish it helps you!

If you still have question, please contact with me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply