Can SPI1 pins 1-4 be used simultaneously with SPI1 pins 91-95 on the K21?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can SPI1 pins 1-4 be used simultaneously with SPI1 pins 91-95 on the K21?

Jump to solution
769 Views
nicholasmarsaw
Contributor II

I need to test out a board I designed for SPI Functionality...however I need to make a mock board to test the SPI protocol/code before my new board comes in. I need to solder wires on to the MC in order to do this, and with how fine the pins are on the K21, I was wondering if I used pins 1 and 4 for CS1 and SIN, along with pins 92 and 95 for SCK and SOUT, if it would function the same do to it all being under the SPI1 peripheral.

Labels (1)
1 Solution
673 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Nicholas,

Sorry for misunderstanding.

As you said that you assign the SPI1 as following:

Pin 1    - SPI1_CS1

PIN 4   - SPI1_SIN

PIN 92 - SPI1_SCK

PIN 95 - SPI1_SOUT

Of course, it is okay, no problem. For example, the SPI1_SCK can be assigned to pin 92 or pin 3, but not both.

BR

Xiangjun Rong

View solution in original post

4 Replies
673 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Nicholas,

Gnererally, we do not recommend customer use mutiple pin for the same peripheral function simultaneously

, because it may lead to damage.

Pls refer to the descriptioin in the RM of K21 with 144 LQFP package.

"

10.2.4 Signal multiplexing constraints
1. A given peripheral function must be assigned to a maximum of one package pin. Do
not program the same function to more than one pin.

"

Hope it can help you

BR

Xiangjun Rong

0 Kudos
673 Views
nicholasmarsaw
Contributor II

Xiangjun thanks for responding. Just to clarify; I am not assigning the same peripheral to more than 1 pin:
Due to SPI1 being accessible from pins 1-7, as well as 91-97 I was planning on accessing different parts at each...

i.e.

Pin 1    - SPI1_CS1

PIN 4   - SPI1_SIN

PIN 92 - SPI1_SCK

PIN 95 - SPI1_SOUT

And as a result of them being on 2 different ports, I would enable to port clocks on each (PTE & PTB), as well as the SPI clock. I am not using 2 pins in operation under the same peripheral function.

So...Is this okay to do then?

0 Kudos
674 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Nicholas,

Sorry for misunderstanding.

As you said that you assign the SPI1 as following:

Pin 1    - SPI1_CS1

PIN 4   - SPI1_SIN

PIN 92 - SPI1_SCK

PIN 95 - SPI1_SOUT

Of course, it is okay, no problem. For example, the SPI1_SCK can be assigned to pin 92 or pin 3, but not both.

BR

Xiangjun Rong

673 Views
nicholasmarsaw
Contributor II

No problem at all! That's what I assumed, but I wanted to make sure before I take next steps. Thanks Xiangjun!

0 Kudos