Can KEIL work with IAR J-Link Lite for Cortex-M debug probe?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can KEIL work with IAR J-Link Lite for Cortex-M debug probe?

跳至解决方案
2,542 次查看
BasePointer
Contributor II

Hi,

 

I want to order tower K60 from IAR. They will provide an IAR J-Link Lite for Cortex-M debug probe.

At the same time, I would like to evaluate KEIL. Can I use same debugger from IAR for also KEIL?

 

Thanks.

 

0 项奖励
1 解答
1,632 次查看
lukas
Contributor III

it doesnt support IAR J-link - when you try to download program - it detect the IAR tool, give back negative message and doest continue with the download

在原帖中查看解决方案

0 项奖励
6 回复数
1,632 次查看
mjbcswitzerland
Specialist V

Hi

 

Keil uVision4 supports the J-Link / J-Trace from Segger. The IAR J-Link Lite is a low speed J-Link from Segger with IAR branding (but fast enough for most work).

 

Keil uVision4 (lastest version) also supports the inbuilt OSJTAG interface (as do all IDEs with Kinetis support) so will work without any external debugger.

 

Regards

 

Mark

 

0 项奖励
1,632 次查看
BasePointer
Contributor II

Do you know that Keil also supports IAR J-Link Lite?

0 项奖励
1,633 次查看
lukas
Contributor III

it doesnt support IAR J-link - when you try to download program - it detect the IAR tool, give back negative message and doest continue with the download

0 项奖励
1,632 次查看
BasePointer
Contributor II

 

Thanks Lukas for this feedback.

0 项奖励
1,632 次查看
mjbcswitzerland
Specialist V

Hi Lukas

 

Interesting. This sounds as though uVision is actively rejecting the J-Link with IAR branding since other programs don't seem to care whether it is a high speed J-Link, low speed J-Link or an IAR packaged one of these.

 

Regards

 

Mark

 

P.S. I'll have a try with an old IAR J-Link Lite once I get back from holiday....

0 项奖励
1,632 次查看
DistiCasMgr
NXP Employee
NXP Employee

Hi,

 

I asked ARM about this today and was told the following:-

 

If the J-Link in question is branded as Segger it will work, if it is branded as IAR, then the embedded IAR firmware stops it from working with Keil MDK.  (So MDK is capable of using it  but IAR won’t let it happen...).

 

Hope that clarifies.

 

Damian

0 项奖励