Can KEIL work with IAR J-Link Lite for Cortex-M debug probe?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can KEIL work with IAR J-Link Lite for Cortex-M debug probe?

Jump to solution
2,562 Views
BasePointer
Contributor II

Hi,

 

I want to order tower K60 from IAR. They will provide an IAR J-Link Lite for Cortex-M debug probe.

At the same time, I would like to evaluate KEIL. Can I use same debugger from IAR for also KEIL?

 

Thanks.

 

0 Kudos
1 Solution
1,652 Views
lukas
Contributor III

it doesnt support IAR J-link - when you try to download program - it detect the IAR tool, give back negative message and doest continue with the download

View solution in original post

0 Kudos
6 Replies
1,652 Views
mjbcswitzerland
Specialist V

Hi

 

Keil uVision4 supports the J-Link / J-Trace from Segger. The IAR J-Link Lite is a low speed J-Link from Segger with IAR branding (but fast enough for most work).

 

Keil uVision4 (lastest version) also supports the inbuilt OSJTAG interface (as do all IDEs with Kinetis support) so will work without any external debugger.

 

Regards

 

Mark

 

0 Kudos
1,652 Views
BasePointer
Contributor II

Do you know that Keil also supports IAR J-Link Lite?

0 Kudos
1,653 Views
lukas
Contributor III

it doesnt support IAR J-link - when you try to download program - it detect the IAR tool, give back negative message and doest continue with the download

0 Kudos
1,652 Views
BasePointer
Contributor II

 

Thanks Lukas for this feedback.

0 Kudos
1,652 Views
mjbcswitzerland
Specialist V

Hi Lukas

 

Interesting. This sounds as though uVision is actively rejecting the J-Link with IAR branding since other programs don't seem to care whether it is a high speed J-Link, low speed J-Link or an IAR packaged one of these.

 

Regards

 

Mark

 

P.S. I'll have a try with an old IAR J-Link Lite once I get back from holiday....

0 Kudos
1,652 Views
DistiCasMgr
NXP Employee
NXP Employee

Hi,

 

I asked ARM about this today and was told the following:-

 

If the J-Link in question is branded as Segger it will work, if it is branded as IAR, then the embedded IAR firmware stops it from working with Keil MDK.  (So MDK is capable of using it  but IAR won’t let it happen...).

 

Hope that clarifies.

 

Damian

0 Kudos