Can I use FRDM-K22F eval board with MK22FN512VLH12 MCU on it to run code built for MK22FN256CAH12 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use FRDM-K22F eval board with MK22FN512VLH12 MCU on it to run code built for MK22FN256CAH12 MCU

859 Views
priya_dwivedula
Contributor III

Can I use FRDM-K22F eval board with MK22FN512VLH12 MCU on it to run code built for MK22FN256CAH12 MCU? I am able to flash the code the eval board but it's getting struck up in startup.c.

Tags (1)
0 Kudos
Reply
1 Reply

788 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

With the default (P&E) firmware on the FRDM-K22 it is not possible to debug another processor, except the device on the FRDM board itself.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply