Hi,
I would like to order K60 tower. We have Cyclone Pro. Can I use it on tower for debugging with CW? Or Do I have to order BDM pod?
Thank you.
Hi
The Tower boards have an integrated OSJTAG debugger on the processor boards. This means that no external debugger is required.
There is also a standard Cortex debug + ETM connector which can be used by external debuggers which conform to this standard. The Cyclone Pro from P+E doesn't support ARM processors as far as I know (only HC08 HCS08, HC(S)12 and Coldfire+/V1).
Regards
Mark