Can I power my whole circuit with the internal USB Voltage Regulator (VOUT33)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I power my whole circuit with the internal USB Voltage Regulator (VOUT33)?

Jump to solution
1,091 Views
m4l490n
Contributor V

If I have a simple device consisting of an MK22FX512AVLH12 and other small devices whose total consumption is not more than 100ma, could I power the whole board using the internal USB voltage regulator (Vout33)?

That would mean connecting the VOUT33 to the K22 VDD which doesn't sound right but I'm not sure.

Anyway, is this possible?

0 Kudos
Reply
1 Solution
1,080 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi m4l490n,

  Please check the datasheet:

 

kerryzhou_0-1619066987148.png

So, your consumption is below 100mA, you can use the VOUT to power on the 3v3, it's OK.

 

Wish it helps you!

Best Regards,

kerry

 

View solution in original post

0 Kudos
Reply
1 Reply
1,081 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi m4l490n,

  Please check the datasheet:

 

kerryzhou_0-1619066987148.png

So, your consumption is below 100mA, you can use the VOUT to power on the 3v3, it's OK.

 

Wish it helps you!

Best Regards,

kerry

 

0 Kudos
Reply