Can I have a BSDL file for the MK66FN2M0VMD18 please

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I have a BSDL file for the MK66FN2M0VMD18 please

1,854 Views
MKW
Contributor I

I have a board I need to bring-up but can't find this file on the web site.

Thanks

Martin

Labels (1)
0 Kudos
Reply
4 Replies

1,657 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi Martin Walton,

I am sorry that this process is taking too long.

I found the document  hope this  works. I had two BSDLin case you have LQFP or BGA.

have a great day.

BR

Jonathan

0 Kudos
Reply

1,657 Views
MKW
Contributor I

Hello Jonathan

Thanks for the files, the BGA file does appear to be a correct match for the device I'm using, however, the actual device reports a different JTAG ID code to that found in the file.

When I scan the JTAG chain with the tool I'm using (XJTAG), I see a device with the id code 0x4BA0_0477, which I belive is an Arm manufacturer code.  This is different from the ID code in the file you sent me, which is 0x0B3E_201D.  Is there something I have to do to get this ID to appear on the scan chain, or some mode I have to put the device in for this to work?

Thanks

Martin

0 Kudos
Reply

1,657 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hello Martin Walton,

Hope you are doing great, You can request the BSDL  files in this page Kinetis Symbols, Footprints and Models|NXP .

Have a great day.

BR

Jonathan

0 Kudos
Reply

1,657 Views
MKW
Contributor I

I have requested the file - does this usually take very long to handle?

It would be good if these files were on the product page along with the data sheets.

Thanks very much

Martin

0 Kudos
Reply