CW 10.2 MQX3.8 and TWRK60N512 demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10.2 MQX3.8 and TWRK60N512 demo

Jump to solution
1,136 Views
JamesTPDI
Contributor II

Can this combination of modules be made to compile, program and run the demo (sensor, LED's Touch, Shell etc..) that comes on the tower system using the P&E multilink universal debugger? I was able to do "Hello world" in CW and the LED flash in IAR. Both running from ram. The full tower demo is a bit more elusive with many compile errors.

 

I have a CW license and the IAR demo and would like to use both for this evaluation. My goal is to look at debug cycle time (edit, compile, program, run to edit time) for a full working application with the two tools and see if the MK60 and tools make sense for us for a new design.

 

Specific directions for this combination would be most apreciated.

 

James

 

 

 

 

 

 

0 Kudos
Reply
1 Solution
1,031 Views
JamesTPDI
Contributor II

Yes it works!

 

You have to change the libary path to 3.8 (even though the demo is located there).

 

James

View solution in original post

0 Kudos
Reply
1 Reply
1,032 Views
JamesTPDI
Contributor II

Yes it works!

 

You have to change the libary path to 3.8 (even though the demo is located there).

 

James

0 Kudos
Reply