CAN communication at KV5x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN communication at KV5x

968 Views
CauTran
Contributor I

Hi everyone, 

I had a problem when I am used CAN communication. 

I am using CAN1 for communication. I have three node ID. Two node is a slave, they have 0x039, 0x010 for send, respectively. And received id is 0x0D3, 0x09C respectively.  And one node is a master. 

There is okay when the slaves transfer data to master or master transfer data for slaves. 

But when slaves and master transfer data concurrently, I see problem. My program see the packet lost at both directions.  when I use candump in linux, I see that problems found when receiving and transmitting meet.

This is my project for can testing. Please focus on rcp_can.c and rcp_can.h on utilities folder.

0 Kudos
Reply
1 Reply

947 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hello @CauTran,

I see that you have another case with the same question, I will follow up on this last one that I mention.

0 Kudos
Reply