CAN MKE06

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN MKE06

Jump to solution
2,944 Views
eliezeroc
Contributor III

Hello people.

How do I start CAN module and how do I send and receive mensgens.

The project already uses MKE06.

Can be at Processor Expert.

Already read all the documentation but it's very complex.

Thank you.

0 Kudos
Reply
1 Solution
2,597 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Eliezer Oliveira Cardoso,

    Actually, the baud rate relate register is MSCAN_CANBTR0 and MSCAN_CANBTR1.

    These codes:

sMSCANConfig.sBaudRateSetting.SJW = BAUD_RATE_SJW;

sMSCANConfig.sBaudRateSetting.BRP = BAUD_RATE_BRP;

sMSCANConfig.sBaudRateSetting.SAMP = BAUD_RATE_SAMP;

sMSCANConfig.sBaudRateSetting.TSEG1 = BAUD_RATE_TSEG1;

sMSCANConfig.sBaudRateSetting.TSEG2 = BAUD_RATE_TSEG2;

is just configure register MSCAN_CANBTR0 and MSCAN_CANBTR1.

CAN_SendItemToBuffer function will send your CAN data, if you test the code on your KE06, you will find it.

The sample code is based on FRDM-KE06, you can test it and combine the KE06 reference manual to understand it.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
10 Replies
2,597 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Eliezer Oliveira Cardoso,

   Actually the MSCAN in KE06 is not complex, you can refer to our KE06 sample code and the KE06 reference manual, it is not complicated to understand.
The attachment is the MSCAN sample code for FRDM KE06, you can refer to it. This sample code is the none PE project.
Please refer to it at first, if you have some points don't understand, you can tell me!
If you want the PE project, I also attached the CW PE MSCAN project for KE06, the name is:KE06_CAN.zip

Wish it help you!

Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,597 Views
eliezeroc
Contributor III

Hello, Jingjing.

First thanks for your help.

I made changes to my hardware and I'm having sign in CAN_TX and CAN_RX. I could not change the BAUD_RATE actually I did not understand how fuciona this calculation.

I need to work at the speed of 150 kbit / s.

#define BAUD_RATE_SJW         SJW_3TQ

#define BAUD_RATE_BRP         0     

#define BAUD_RATE_SAMP        0           

#define BAUD_RATE_TSEG1       TSEG_10 

#define BAUD_RATE_TSEG2       TSEG_7  

#define BAUD_RATE_CLOCK       8000000L

#define Baud_RATE             BAUD_RATE_CLOCK/(BAUD_RATE_BRP+1)/\                                                              (BAUD_RATE_SJW+1)/(3+BAUD_RATE_TSEG1+\

                              BAUD_RATE_TSEG2)

0 Kudos
Reply
2,597 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Eliezer Oliveira Cardoso,

     Actually, in the reference manual,  there have the calculation formula, if you want to get 150Kbit/s, and use 8Mhz as the clock source, you should follow this formula:

Bit time= (1+ Time Segment1 + Time Segment2)(1+BRP)/8Mhz

Take care:      8<= (1+ Time Segment1 + Time Segment2)<=25

So, you can configure it like this:

45.jpg

BPR=2

TSEG1= 9

TSEG2=8

Wish it helps you!

If you still have question, please let me know!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,597 Views
eliezeroc
Contributor III

Thank Jingjing.

I will use your example.

0 Kudos
Reply
2,597 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Eliezer Oliveira Cardoso,

You are welcome!

If your question is solved, could you click the Correct Answer button? Thank you!

Best Regards,

Jingjing

0 Kudos
Reply
2,597 Views
eliezeroc
Contributor III

Hello Jingjing.

Sorry to bother you again, it is the first time working with CAN communication.

I'm having trouble understanding the way the code was written.

To which register I should spend the calculation value of BAUD_RATE?

At startup of CAN have the following code:

sMSCANConfig.sBaudRateSetting.SJW = BAUD_RATE_SJW;

sMSCANConfig.sBaudRateSetting.BRP = BAUD_RATE_BRP;

sMSCANConfig.sBaudRateSetting.SAMP = BAUD_RATE_SAMP;

sMSCANConfig.sBaudRateSetting.TSEG1 = BAUD_RATE_TSEG1;

sMSCANConfig.sBaudRateSetting.TSEG2 = BAUD_RATE_TSEG2;

To send a messages exist, simply call the CAN_SendItemToBuffer function (mscan, & sCANTxItemInfo, & sCAN_TxBuff); ?

My message I carry for & sCANTxItemInfo?

Thank you?

0 Kudos
Reply
2,597 Views
eliezeroc
Contributor III

each start time and change the value displayed.

img_1.pngimg_2.pngimg_3.png

0 Kudos
Reply
2,597 Views
eliezeroc
Contributor III

Hello Jingjing.

I managed to set the baud rate, the cam is sending data.

I would like to help me find where I set the device ID and in which I write variable values from my sensor to send by CAN.

Thank you.

0 Kudos
Reply
2,598 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Eliezer Oliveira Cardoso,

    Actually, the baud rate relate register is MSCAN_CANBTR0 and MSCAN_CANBTR1.

    These codes:

sMSCANConfig.sBaudRateSetting.SJW = BAUD_RATE_SJW;

sMSCANConfig.sBaudRateSetting.BRP = BAUD_RATE_BRP;

sMSCANConfig.sBaudRateSetting.SAMP = BAUD_RATE_SAMP;

sMSCANConfig.sBaudRateSetting.TSEG1 = BAUD_RATE_TSEG1;

sMSCANConfig.sBaudRateSetting.TSEG2 = BAUD_RATE_TSEG2;

is just configure register MSCAN_CANBTR0 and MSCAN_CANBTR1.

CAN_SendItemToBuffer function will send your CAN data, if you test the code on your KE06, you will find it.

The sample code is based on FRDM-KE06, you can test it and combine the KE06 reference manual to understand it.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,597 Views
eliezeroc
Contributor III

Ok, I will study the example of KE06.

Thank you.

0 Kudos
Reply