CAN Bus monitoring Tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN Bus monitoring Tool

2,940 Views
ekta_rathod
Contributor II

Hello,

I am using S9KEAZ64A kinetics controller for CAN data transmission and reception. To observe the data on CAN bus, BUSMASTER open source output terminal is being used by connecting PEAK CAN adapter  and also tried for Kvaser CAN analyzer but could not get the data on BUSMASTER, as written code is correct (checked the voltage level on CANBUS).

Is there any other CAN adapter or Output terminal where I can monitor the data on CAN Bus?

Please suggest me the solution.

Regards,

Ekta

0 Kudos
Reply
3 Replies

2,920 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Ekta,

There are many CAN analyzers in the market. I use CANalyst-II.

 

Regards,

Jing

0 Kudos
Reply

2,912 Views
ekta_rathod
Contributor II

Is it necessary to connect terminating resistors on CAN analyzer end ?

0 Kudos
Reply

2,905 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

No it can't connect resistor.

 

Regards,

Jing